Other Parts Discussed in Thread: XTR110 , OPA454 , OPA445 , OPA453 , OPA452
Hello to all,
Now I intend to apply XTR110 as voltage-controlled current source to a neuromuscular electrical stimulation (NMES) device. Input signal is pulsed biphasic, frequency…
Other Parts Discussed in Thread: XTR110 , XTR111 Hello, we would like to convert a 0-4.096V to 4-20 mA. Before to invest time on this design could you answer these questions about the circuit published in the XTR110.pdf figure 5 : - If we modify the connecton…
Other Parts Discussed in Thread: XTR110 , XTR116 , XTR105 , RCV420 , XTR112 , XTR117 , XTR111 Hi
I wish to experiment with this device, XTR110.
If it is used in a analog output configuration (4-20mA), how can it use the 2 wire for self power?
In other…
Other Parts Discussed in Thread: XTR111 , XTR110 I am willing to use XTR110 or XTR111 for voltage controlled current source (or sink) application in a neurophysiology research application. I have two questions:
1. Is there any Spice model to use under…
Other Parts Discussed in Thread: XTR110 I have several XTR110 ICs on pc boards that will not put out 4mA when powered up. If I touch the Vref_sense pin (12), the output will start. I have resoldered all the pins and checked all the connections.
The circuit…
Shaival,
You are using the XTR110 in the correct type of application.
The XTR110, a three-wire transmitter, is used in mains-powered equipment to send a 4-20mA signal to a remote device. Often the remote device is an actuator of some type such as in…
Other Parts Discussed in Thread: XTR110 I'm trying to set up an XTR110 op amp to convert a 0-10V to 4-20mA signal for a electronic pressure regulator. I've wired the circuit as shown in Fig. 1 of the white pages, with the substitution of two PNP transistors…
Other Parts Discussed in Thread: XTR110 , RCV420
The purpose of this circuit is to provide some form of
manual offset for a 4-20mA driven gauge connected directly to a sensor. A 1-turn
offset potentiometer (R1 on the XTR110…
Other Parts Discussed in Thread: XTR110 Hello,
Can anyone tell me the maximum and typical voltage at pin 14 (gate drive) of XTR110?
I can't find it in the datasheet.
Poh Leong
Other Parts Discussed in Thread: XTR110 I am tryng to use an XTR110 chip with 0-5V input and 0-20mA output. I have hooked up the circuit as shown below, but I get either 0 or 49.8 mA out depending on whether the circuit is hooked up with pin 1 and pin…