Part Number: XTR116 Other Parts Discussed in Thread: XTR111
When I first energize, the XTR116 draws 80 ma current. Since there is too much voltage drop over the 250 ohm resistor, the supply voltage (V + and IO) of the XTR116 drops below 7.5 volts…
Part Number: XTR116 Other Parts Discussed in Thread: XTR115 Hi Team,
Some failures comes up with the phenomena that device can not generate the right current with different input and loop current stays at maximum. FA report shows the failure is caused…
Part Number: XTR116 Are there any app notes on the XTR116 that discuss the selection purpose, selection criteria and guidelines for the output capacitor. The datasheet doesn’t mention how to select this component, what effect the value has on the output…
Part Number: XTR116 Other Parts Discussed in Thread: ISO7310C Hi,
I made the following circuit from Collin Wells' blog:
Everything works well except for aprox. 100uA overshoot pulses on output current. Frequency was the same of PWM (10Khz):
I couldn…
Part Number: XTR116 Other Parts Discussed in Thread: DAC121C085 , XTR117 , ISO1541 Hello,
I am using XTR116 with DAC121C085. I have only one power source and 2 wires. Is that a normal operation ? +24V input for loop+ and loop- connected to that source…
Part Number: XTR116 Other Parts Discussed in Thread: XTR115 , Hi,
Can we eliminate below Q1 if thermal condition is not problem?
Best Regards,
Kuramochi
Part Number: XTR116 Hi,
Noise is specified 0.6uVpp on the datasheet.
How much does this contribute to output current noise?
I would like to know the equation to calculate it.
Best Regards,
Kuramochi
Part Number: DAC8740H Other Parts Discussed in Thread: XTR115 , , XTR117 , XTR116 In your reference design for the DAC8740H family devices, I see you use separate a op amp, regulator, and voltage reference for the 4-20mA driver portion of the circuit. I…
Part Number: XTR116 Other Parts Discussed in Thread: XTR117 , XTR111 Hello,
I am looking for a 4-20mA transmitter to connect to the output of my DAC. I have seen the XTR116 and XTR117 and was wondering if they would work with a 4 wire system? If not would…
Part Number: XTR116 Hi Sir,
Pls reference below circuit, this circuit is work normally and the output voltage (VRL)= 5V (20mA*250ohm). If I swinging the Micro-USB cable, the voltage will increase to 7V and will latch till re-plugin this cable.
I think…