Part Number: XTR116 Hi,
Can you please share the continuous output current of VREG pin of XTR116.
Its short circuit current observed as 12mA in the datasheet.
Part Number: XTR116
I have built and deployed many boards out into the field using the XTR116 in an isolated configuration.
This design has always worked well and is stable on the bench, but now I being told that the the 4-20 output occasionally "drifts…
Part Number: XTR116 Other Parts Discussed in Thread: XTR115 Hi Team,
Some failures comes up with the phenomena that device can not generate the right current with different input and loop current stays at maximum. FA report shows the failure is caused…
Part Number: XTR116 Are there any app notes on the XTR116 that discuss the selection purpose, selection criteria and guidelines for the output capacitor. The datasheet doesn’t mention how to select this component, what effect the value has on the output…
Other Parts Discussed in Thread: XTR105 , XTR117 , XTR111 , XTR115 , XTR116 , TLV9002 , TMP61 Hello Everyone, I have RTD module which taking the input from the user. With the different combination of resistance and XRT105 2 wire current transmitter 4-20 mA. Now…
Part Number: XTR116 Other Parts Discussed in Thread: ISO7310C Hi,
I made the following circuit from Collin Wells' blog:
Everything works well except for aprox. 100uA overshoot pulses on output current. Frequency was the same of PWM (10Khz):
I couldn…
Part Number: XTR116 Other Parts Discussed in Thread: DAC121C085 , XTR117 , ISO1541 Hello,
I am using XTR116 with DAC121C085. I have only one power source and 2 wires. Is that a normal operation ? +24V input for loop+ and loop- connected to that source…
Part Number: XTR116 Other Parts Discussed in Thread: XTR115 , Hi,
Can we eliminate below Q1 if thermal condition is not problem?
Best Regards,
Kuramochi
Part Number: XTR116 Hi,
Noise is specified 0.6uVpp on the datasheet.
How much does this contribute to output current noise?
I would like to know the equation to calculate it.
Best Regards,
Kuramochi
Part Number: XTR117 Other Parts Discussed in Thread: XTR115 , XTR116 The datasheet specifies input referred noise as 0.6uVpp 0.1-10Hz.
I want to use the loop to transmit signals into the kHz range.
Do you have a specificaion or graph showing input referred…