Part Number: XTR300 Hi team, I'm looking at Figure 8 of the datasheet. I know this data is a typ value. How much variation can you think of MIN/MAX of this value? It does not have to be a guaranteed value. Sincerely. Kengo.
Part Number: XTR300 Hi team, Is it possible to control Idrv in voltage output mode? If yes, does the output swing widen when the IDRV is set to 15mA or higher? Sincerely. Kengo.
Part Number: XTR300 Other Parts Discussed in Thread: XTR305 , , TIPD155 Dear TI Team Our customers are requesting Vin vs Vout measurement data when using the XTR300 and XTR305 in voltage output mode. (To understand the error of Vout with respect to Vin …
Part Number: XTR300 Other Parts Discussed in Thread: , TINA-TI I'm currently evaluating the XTR300 using the evaluation board. I noticed that with the default board configuration any input signal above 50Hz gets distorted and hence at 1KHz the input/output…
Hi Alen,
We haven't heard from you in a while. We hope the issue was resolved. Closing this thread now. Reply to re-open if you have any additional questions.
Part Number: XTR111 Other Parts Discussed in Thread: XTR117 , XTR300 Hi,
Greetings!!
We are using XTR111 and XTR117 in 3 wire transmitter and loop power transmitter (2 wire).
As I understand 3 wire transmitters are working in current source configuration…
Part Number: XTR300 When operating the XTR300 in open loop mode, we notice that Icopy does not output to Imon. Please advise how to internally connect Imon to the current mirror in open loop mode.
Part Number: DAC8564 Other Parts Discussed in Thread: OPA333 , OPA317 , OPA391 , OPA191 , XTR111 , XTR300 HI SIR
I want to design a 4-20mA Function which use the DAC8564,
Did you have suggestion AMP for this?
thanks
HI Joe,
The XTR111 is a similar 3-wire analog current output transmitter, that can operate with a single unipolar +24V supply, however, the functionality is not exactly the same. The main difference is the XTR111 is used primarily as a current output…