Part Number: CC1101-CC1190EM869RD Other Parts Discussed in Thread: CC1101 Tool/software: I have been trying to get a package from the RF Link Transmitter - 434MHz - WRL-10534, an RF remote, and a Screw on TPMS sensor. So far I am not able to receive any…
Hi TI-CSC,
As far as I understand, Pin 2 is just there for sensing the Vdd voltage. I believe you should also connect Pin 9 to Pin 2, and the CC1101 Vdd.
Regards,
Arthur
Part Number: CC1101 Other Parts Discussed in Thread: CC1311R3 , CC110L Tool/software: Hello,
We're working on a project to do the following:
Sensor-> XMIT data (using CC1101 or other) -> Receive and display data on a remote unit.
This should…
Part Number: CC1101 Other Parts Discussed in Thread: CC1310 , LAUNCHXL-CC1310
Hi, I'm trying to communicate a LAUNCHXL-CC1310 board with a custom board which uses a CC1101. I'm using the custom board on a proyect based on MPLAB, on the other hand I…
Part Number: CC1101 Tool/software:
Hi everyone,
I've been reviewing the CC1101 datasheet, specifically section 19.7 RX Termination Timer . It mentions:
"For ASK/OOK modulation, lack of carrier sense is only considered valid after eight symbol periods…
Hey, community,
I have been eagerly awaiting some replies to this post. In case there is any confusion caused by the Chinese characters in the attached images, here are some notes:
Explanation of the Oscilloscope Images:
In the attached oscilloscope images…
Part Number: CC1101 Other Parts Discussed in Thread: TEST2 , Hello siri, I am facing couple of issues. It would be very helpful if you help me out. 1.) While sending data device stuck in line while(!(PIND & (1 <<GDO2 ))); "Wait for GDO2 to be set…
Part Number: CC1101 Other Parts Discussed in Thread: TEST2
Tool/software:
Hello,
We are using the CC1101 as a transmitter & a receiver. There are multiple CC1101 is configured as a transmitter with data whitening ON & we had configured one CC1101 as…
Part Number: CC1101 Tool/software: Hi, we are struggling to get a CC1101 to work (915MHz band). The schematic should be the same as the ref design (see below). When probing the RF out pins of the CC1101 while telling it to transmit, we see a strange …