Part Number: CC1101 Other Parts Discussed in Thread: TPS62730 Tool/software: Hello,
We have made an application with a CC1101 voltage regulator, which is used TPS62730. We have been getting <1uA for specific TPS62730 regulator. but we are getting 25uA…
Part Number: CC1101-Q1 Tool/software: Below are two snapshot from the datasheet regarding the data rate,
From Introduction section, it indicates the maximum data rate is 250kBaud,
From the '3.8 Data Rate Programming' section, it states that "The data…
Hi Felipe,
This is a very interesting conversation and I would be interested to know how well this works for you.
We have been using the CC1200 to receive bi-phase encoded data starting with FFFE for many years, but have used the CC1200 just as an 'RF…
Part Number: CC1101 Other Parts Discussed in Thread: TEST2 Dear Team, I am currently utilizing the CC1101 chip, where I have initiated the power-down mode by implementing the following configuration:
void CC1101_PowerDown()
{
SpiStrobe(CC1101_SIDLE…
Part Number: CC1101 Tool/software: Hi,
I'm currently working on a project with the CC1101 transceiver, but I'm stock at one point.
The chip is not sending data stored in the TX FIFO.
Overall, everything is working properly between the controller…
Part Number: CC1101 Tool/software: Hi folks,
I am encountering a problem regarding the setting of the CS absolulte threshold in Async mode, which is a must for compatibility with various old devices.
In my application, I need to set the threshold dynamically…
I do not understand what you are doing in the code you have provided, and I am unsure what you are asking about in the post.
In the code you are for example writing to 59 registers, but I gave you a list of 26 register you should use?
Why are you writing…
Hi,
With the CC1101, the best option would be to use the 868 MHz balun; which goes into a SPDT switch. With the "A" switch option, there should be a 433 MHz LPF and on the "B" switch option there should be a 868 MHz LPF. Then these signals should…