Al,
The reference design that we have available on our website covers from 860-928MHz without changing anything. Please do note that the antenna is not included on this reference design as it does require changes to tune from 860 to 915MHz.
http…
Charith,
Yes, SmartRF Studio is designed to be used as a demostration tool. It comes with basics settings and basic packet error rate test software.
You need the entire kit as show in this link for it to work with CC1101 family of transceivers.…
The development kit does come with 2 of everything. http://focus.ti.com/docs/toolsw/folders/print/cc1101dk868-915.html
Can it do what you want? Need to know the data rate to answer that, at the higher data rates you will need directional antennas to…
Hi,
Recommend to perform some field test in your environment with the kits that are available. Agree that sub 1GHz is the best option and would start to evaluate your application with 868 MHz. By performing the field tests with the kits then you can…
Other Parts Discussed in Thread: MSP430F5438 , CC1101 Hello,
I am building an automated blood pressure monitor for a project at school and need some pointers for the wireless portion of the project.
My designed PCB will have a connection for the…
JB,
I am having a hard time finding any information about sync words and preambles used by the Zarlink devices. I say this because although the CC1101 has a flexible and programmable sync word and preamble strategy there could be cases where it just…
Other Parts Discussed in Thread: CC1101 Hello,
I have a CC1101DK868-915. It appears that when using the CC1101DK that one can generally experiment with the PER tester application and RFStudio.
It appears that one can download a new program to the…
Hi Aloha,
I noticed you sent me some questions about the CC2431. I'll try to answer them here (for the benefit of others to see as well, hopefully without extraditing too much):
1) You asked if this was suited for your project <xyz with product description…