Part Number: TPS563300 Hi Team,
Customer said that there are the differences between their measurement data and the datasheet on the negative voltage of SW pin by load current. Please check the attachment below and let me know the reason why. And please…
Hi Gui,
Thank you very much for your supports.
Could I ask you an additional question about TPS92641? If I should ask it on new thread, please let me know.
The customer question is the below.
Q. They are producing many type of LED light source…
Hi Kaiji,
Kaji@PAN said: And this symptom occurs when VIN is turned on and off repeatedly.
Thanks for providing the critical information.
I verified on EVM and similar waveforms were observed. This kind of negative SW voltage happens during shutdown…
Part Number: TPS55340 Hi
I want to improve the negative voltage of the sw pin (red on the waveform photo) Please let me know the points that I can improve.
-spec-
Input - DC26V
Output - 29V / 0.3A
Thanks
Part Number: TPS61169
Tool/software:
Dear Team,
My customer is evaluating the TPS61169 at LCD Panel LED Backlight driver application. And they measured around -1.3V negative undershoot voltage at SW pin which is larger than -0.3V of absolute maximum…
Part Number: LM63615-Q1 Tool/software:
I am measuring SW node voltage of LM63615DQPWPRQ1, I could witness the sudden dip in rising edge of sw node and it is rising again. can you please explain why this behavior and how to mitigate this
Part Number: TPS659128 Tool/software: Hi Team,
Could you please help to check the negative voltage spec in SW for each Buck?(DC-DC1 to DC-DC4)
Thank you
Yishan Chen
Part Number: TPS54302 Tool/software: Hi,
A my account measures that negative peak voltage on SW pin of TPS54302 is <-0.3V@156nS, is there any risks for TPS54302?
note: the GND loop is as the following.
ch1: SW.
Emma Wang said: My customer still want to know, if there is an equivalent series back 2 back diode from SW to GND for this device.
I don't believe there is a back to back diode on the SW pin.
Emma Wang said: What is the restriction SW can only stand…
Part Number: TPSM8D6C24 Tool/software: Hi team,
We measured the spike voltage of the SW node at different temperatures.
At low temperatures, spikes exceeding 20V were observed.
It appears that the clamping by the protection diode is not working…