Other Parts Discussed in Thread: UCD3138 ****UPDATE****
The process for receiving the UCD3138 family training labs has changed. Follow the link below for more information:
Get UCD3138 Family Firmware Training Labs
****/UPDATE****
The UCD3138 Training Labs…
The UCD3138 device was designed to work with the Phase Shifted Full Bridge. The High-performance Isolated Power team is always working on new topologies that can be controlled by the UCD3138. In fact, a Phase Shifted Full Bridge EVM will become available…
Part Number: UCD3138ALLCEVM150 Other Parts Discussed in Thread: UCD3138A Hello,
I'm using "UCD3138ALLCEVM150" evaluation board. monitoring ucd3138a with " Fuison Digital Power Studio". I have trouble with changing switching frequency on design. Attached…
Hello, Amiel,
data2-15-21.zip 400V48V21A2-15-21DC-DC LLC @ Address 89d Project.xml
The results are as follows:
1. When re-install, start, open the LLC sample project, close without editting, and re-open in admin mode, the error did not occur.
3. Version of…
Hello Ti member,
I need source code of following projects
PFC EVM 026
LLC EVM 028
Could you send files to me, thanks!
My email address : m9807c02@gmail.com
Best Regards.
SK Huang
Other Parts Discussed in Thread: UCD3138 How can I control the 4-wires fan in a closed loop with UCD3138 device? Namely, I need to measure the speed of the fan and control the duty cycle according to the temperature change. In other words, I want to use…