I know that these three, if I am not wrong, can operate between -10 V and +10 V. But are they stable? I mean, what is the error that I can expect once I establish that voltage ?
I know that these three, if I am not wrong, can operate between -10 V and +10 V. But are they stable? I mean, what is the error that I can expect once I establish that voltage ?
Hallo Team,
I am facing difficulty with DAC8562TEVM board. I am using SPI bus to communicate with the DAC. I powered the DAC externally with 3.3V, LDAC is grounded, CLR is pulled high. After powering up the DAC, I provided the…
I'm trying to run the DAC8562TEVM board with an FTDI USB to SPI converter UMFT4222EV-C and DXP and I get the "waiting for USB" hang.
Is it possible to run this setup…
hi,
i was wondering if anybody got DAC8562TEVM Board working with MMB0 Board. technical documenation describes that it can be used with DXP Software. i downloded DXP and connected MMB0…
Hi,
i have DAC8562TEVM Board attached with MMB0 Board. on DXP software i cant find DAC named DAC8562T but there is DAC8562. would DAC8562.xml file work for DAC8562T Device?
kind regards…