Hello Team,
We are using TLC7226 for one of our DAC application. We are using this DAC to control some loads which works on 0-10 volts analog voltage.
We are able to control 5 devices in one channel with each DAC, but when connected…
Hello Team,
We are using TLC7226 for one of our DAC application. We are using this DAC to control some loads which works on 0-10 volts analog voltage.
We are able to control 5 devices in one channel with each DAC, but when connected…
Hi
What is the HIGH and LOW Voltage levels for Control signals A0,A1,WR?
In recommended operating conditions table,Vih=2V min and Vil=0.8V max .Does it condition apply for DB0-DB7 as well as A0,A1,WR?
Regards,
Deebanmadhu
May I know what is the junction to board/case/ambient thermal resistance, and the maximum junction temperature for TLC7226IDW?
Hi,
Presently using TLC 7226CN DAC IC.
I want to know in DAC chip AGND & DGND must be separate in layout? What if both are shorted.
This IC is frequently failing after 4-5 days of operation,no heating found,operated under recommended…
The TLC7226C outputs connect to max301 directly. Sometimes the four outputs change from operating voltage to 0V . I can confirm that Mcu do not control it. What happened will the output reset to 0V?
Hello,
I would like to make a ramping voltage from approximately 0.3VDC up to approximately 1.0VDC.
To accomplish this I decided to try out the TLC7226C from TI. I was able to get this chip to ramp from 0 volts to…