Tool/software:
Hello.
I wanted to calculate the DC/DC buck converter circuit for the TPS40425 chip using the WEBENCH POWER DESIGNER tool. In the input data for the calculation, the input voltage is only available in the range of…
Tool/software:
Hello.
I wanted to calculate the DC/DC buck converter circuit for the TPS40425 chip using the WEBENCH POWER DESIGNER tool. In the input data for the calculation, the input voltage is only available in the range of…
Hi Teams,
In WEBENCH@ POWER DESIGNER, I select TPS40425 (buck controller with SPS) in DC/DC Power Designs. TPS40425 is a two phase controller combined with two SPS (smart power stage). In DC/DC Power Designs, TPS40425 is always designed…
Dear
I am currently looking to program the TPS40425 device using the PMBus protocol. However, I am unable to utilize software such as FUSION_DIGITAL_POWER_DESIGNER for this purpose.
I was wondering if there is any datasheet available…
Hi team,
Our customer is using TPS40425 in server product right now
But customer would like to know the next gen. or any new design by TPS40425 similar
As customer ask, please help to provide part number or solution
BTW: The new…
Hello,
I'm closing this thread as resolved. Please open it again if you have further question.
Regards
How could PMbus Vout under smart power mode?
Also, what is 21h register stand for?
Thanks
Hi Team,
The customer report that the TPS40425 will enter the OTP when the device is only 60 degrees, we think that it should be they add the pull low resistor (PR6 and PR30…