Hi Andy,
Here I attach the log files of charge and discharge:
In the attachment, file ChargeLog-00, as you can see the first charge and discharge cycle the the FCC and RC are not equivalent. Where as in the second cycle (Charge and Discharge) the…
Part Number: BQ27742-G1 Tool/software: Hi team,
Customer feedback battery pack will randomly trigger ISD fault after completing charge. We record log for your reference. And my question is that is selfdischargecurrent accurate? how often selfdischargecurrent…
Part Number: BQ27542EVM Tool/software: Dear TI support team,
I am using the BQ27542 for a discharge test and found that the SOH suddenly drops.
Why did the SOH suddenly drop from 100 to 97 and then further decrease to 93? After starting charging…
Thanks, Jim, that helps a ton. I've been working with the DAC outputs thus far, so I'll start there to make sure I understand and to see what might be happening in my outputs.
In the format pattern, the first number is the MSB (+X) or LSB (-X) for the…
Hello Wyatt,
Would you please check the attached log for the unit that have detected OC last week I logged DSG->CHG->DSG but OC haven't be detected through the cycle?
Kindly I am waiting you advice whether if this log have any explanation to this…
Part Number: LMX2592 We've been using the LMX2592 Synthesizer for several years. Looking at the RF power output in detail, we see shifts in the output at ~1200MHz to 1700MHZ & 3400MHZ. We assume this is due to different internal VCOs being used. I have…
Hi Ammar,
Yes,If we turned off notification then connect devices connections are stable with 3-4 connections also. But when some data transfer going on we are getting connection failed.
Please check below sniffer logs with 2 connections. If we increase…
Part Number: BQ27Z746 Hi Team,
Could you please explain the mechanism of RSOC reporting 0 for the impedance tracking algorithm gauge, and the relationship between TD, FD, Term Voltage and Reserve Cap-mAh? The customer reported a problem that when the…
Part Number: BQ34Z100-G1 Hello Sir:
We are using BQ34z100-G1.
When we are trying to do low temp log tested for Rb table, the temperature from 25 degree down to 0 degree
Then we can see the I2C SDA will latch low about 1 sec two times.
Please refer…