X038-32( 48 )29(X038 电芯测试)(2024-09-12 15_22_22) (2)(2).xlsx Hi Adrian,
We tested it with cell. Is that the right way to test it?Attached is the raw data,please refer,thanks!
Thanks Wyatt for the explanation.
Attached you can find the .xlsx file where you can see how these parameters (DOD Passed Q, DOD Time, DOD0,QmaxDOD0, QmaxPassedQ and Qmax Time) become 0 when full charge is met. (row 1136 in file) bq34z100_SoH_calc.xlsx…
Part Number: BQ34Z100-G1 Other Parts Discussed in Thread: GPCRA0 Tool/software: Hi, Below test was performed on a battery with TI characterized chemID-4190 ( 0% err )
The battery was set to 'rest' after discharging up to 50% SoC for ~four days. There…
Hi Karthik,
Thank you for your reply.
My customer executed following procedure you advised.
1
2
3
4
5
cd build
. conf/setenv
MACHINE=am57xx-evm bitbake -c cleanall qtwebengine
MACHINE=am57xx-evm bitbake qtwebengine…
Hi Wyatt,
Sorry for the last message and the misleading nomenclature. Cx corrected the data as follows: 1) Design Capacity: 2000 2) Design Energy: (Capacity/10)*37 = 7400 3) Terminate Voltage: 3000 Taper Current: 58 -> Used just to calculate the Taper…
Part Number: BQ78350 Hello team,
I am sending email to inquiry about bq78350’s CEDV update
My customer used default GG file and only changed EDV voltage like attached PPT file
However, when customer test charge/discharge, RSOC is updated with…
Hi Sammi,
Thank you for your support. Can you try these files?
2821.[log] ChenID=1297, Charge Volt=3950mV, Term Volt=3500mV(After learning).xlsx
[gg file] ChenID=1297, Charge Volt=3950mV, Term Volt=3500mV.zip
[srec] ChenID=1297, Charge Volt=3950mV…