Meera,
Here are a couple of options that you can use to further evaluate the ADS1118.
First, the ADS1118EVM does have the source code available, but I'm not sure what form it's in. It may actually be a LabView project. If you go to the EVM product folder…
Hi aatif,
I'm not aware of am ADS1118 specific library that might help you, but is is a relatively simple SPI type device. Have you looked through the source code associated with the 430BOOST-ADS1118 ?
Amy,
I'm sorry I didn't see this earlier.
As Bob had mentioned in a previous post, it seems like a timing issue from sending the TX buffer contents. I'm not sure if this will help, but there is at least a template available on how to read the…
The following resources, although not using the exact device requested, demonstrate MSP430 SPI communication with an ADSxx ADC
e2e.ti.com/.../474562
www.ti.com/.../430boost-ads1118
www.ti.com/.../BOOST-ADS7042
Regards,
Ryan
Sakthivel,
We don't have any specific code to work with the AT23UC3A1256, however there are a few examples of code to draw from.
First, we do have an ADS1118 BoosterPack, that shows an example board controlled by an MSP430G2553 device. There is…
There is a fully-working demonstration of the 430BOOST-ADS1118 using a MSP-EXP430G2 LaunchPad: www.ti.com/.../sbac121
The G2 LaunchPad is very cost-efficient and I would highly recommend getting one to jump-start your project. You can then use this…
The schematic in the 430BOOST-ADS1118 User's Guide shows that the only unused header pins on the G2553 LaunchPad are XIN/XOUT/TEST/RST, and P1.1 (TXD), P1.2 (RXD), and P1.3 (S2).
Uday,
I don't think we have anything written in python. There is something written in c though.
The ADS1118 has a booster pack for the MSP430G2553 and there's information and code here:
www.ti.com/.../430boost-ads1118
Joseph Wu
Hi Fakhruddin,
TIPD109 shows the temperature sensor placement relative to the cold junction. This board is very small so unfortunately it doesn't show the thermal isolation. There is an ADS1118 BoosterPack (430boost-ads1118) that shows a thermally…
Hi,
As described here: http://www.ti.com/tool/430boost-ads1118
The 430BOOST-ADS1118 Booster Pack provides a quick and low-cost solution to evaluate and develop the ADS1118 for temperature measurement applications using type K thermocouples. This booster…