Part Number: 430BOOST-CC110L Hi everyone,
I am working on a project using one 430BOOST-CC110L as an emitter along with Tiva C TM4C123 and I want to use Anaren ATC-Booster Stack Lite to visualize the transmitted frames. It is possible to use Tiva C TM4C1294…
Part Number: 430BOOST-CC110L I just purchased one 430BOOST-CC110L plus two MSP430G2ET Launchpads to test 915MHz Wireless transmission between MSP430 devices. Both of the MSP430G2ET kits were tested and worked in their original configuration.
Then I replaced…
Part Number: 430BOOST-CC110L i am constructing a star network using 430BOOST-CC110L where at the host i need to upload data to cloud .. i am using MSP-EXP430G2ET with 430BOOST-CC110L as a node... if i can connect 430BOOST-CC110L to cc3200 i can directly connect…
Other Parts Discussed in Thread: MSP430FR5969 Hi,
I have MSP430FR5969 launch pads and a set of 430BOOST-CC110L for a wireless network. My computer detects the launch pads precisely while they are connected alone (without rf boosters on them). When I connect…
Part Number: 430BOOST-CC110L According to BoosterPack Checker the 430BOOST-CC110L is compatible with EXP432P401R and EXP430F5529LP ( I have both). However the AIR BoosterPack kit has a preprogrammed 5523 chip (20 pin DIP)
.How do get this firmware onto…
Part Number: 430BOOST-CC110L
Hi,
I developed Radio communications based on the TI/Anaren RF CC110L.
The circuits were doing well in the absence of obstacles. However, when I put my board into a vehicle, I lose receiving packets.
SO I proceeded to use a…
Part Number: 430BOOST-CC110L Hello,
I'm developing Rf communications based on the TI CC110L.
At this stage, I'm trying to verify the Packet error rate depending on the distance between the transmitter and the receiver.
My setup contains the following…
Part Number: 430BOOST-CC110L Hello,
I am working with msp430g2553 with cc110l booster pack on energia
My query is regarding this function
----------Radio.begin(0x01, CHANNEL_1, POWER_MAX);---------------
Here i found that the second parameter of this…
There is another problem with the cc6
I can not import the project from the directory D:\Firmware\CCS correctly .
and when I import it i can not read or write on it .
what i have to do ?
x v
Other Parts Discussed in Thread: CC110L Hello,
Does the CC110L has also restrictions due to legislation as f.e. Sigfox has: frequency of sending messages is limited and payload size as well?
Thanks. Guy