Part Number: 5-6KINTERFACE
Dear TI
At present, the measured data of EMC current exceeds the standard. The detailed test steps are shown in the attachment. The interference sources obtained in the experiment are 1.7M apart. The interference sources…
Part Number: ADS8323EVM Hi Team,
My customer is using ADS8323 for their application 10 years ago. And now we met some issue and need EVM for debugging.
I've applied the ADS8323 EVM but no base board information. http://www.ti.com/tool/ADS8323EVM
I…
Hi Mohamed
I'm not aware of any single board solutions from TI that have everything you need.
One potential combination would be the following:
DAC8803EVM
5-6KINTERFACE
TMDSDSK5416 TMS320C5416 DSP Starter Kit (DSK)
Best regards,
Jim B
Hello Rez,
Unfortunately, currently we do not have an ADS8332EVM kit with a GUI or ADCPro plug-in that you can directly connect to the PC. This EVM can be interfaced with the 5-6k interface board and one of the DSP kits for firmware development (TMS320C6000…
Hi Akash,
Check out the 5-6Kinterface board (http://www.ti.com/tool/5-6kinterface) - this should mate up with the expansion headers on the TMDSK6455 and will allow you to plug the ADS1258EVM into the serial ports found on the peripheral expansion connector…
Other Parts Discussed in Thread: 5-6KINTERFACE , ADS1605 , TMS320C6416 Hello at all,
My name is Christoph Winterholler and I am doing my diploma project with an ADC and a DSP.
I use the following hardware: ADS1605EVM (5MSPS/16Bit) with 5-6KInterface Board…
Other Parts Discussed in Thread: TMS320C6455 , 5-6KINTERFACE , DAC8552 , ADS8406 Hi ,
Would like to seek advice on tools return /repair policy on the following boards .
Kindly direct me to the route /email or website .
Below boards was purchased by one of…
Hello Avraka, Not all evaluation modules are available as a kit with motherboard and software. Typically, the evaluation modules with motherboard and computer hardware have the “-PDK” termination. I checked the ADS8519 product folder, and there…
Hello Alicia,
Use the following link in case you need to order a “5-6k interface” board or find more information about it:
http://www.ti.com/tool/5-6kinterface
Regards,
Other Parts Discussed in Thread: ADS8361EVM , ADS8361 , 5-6KINTERFACE Dear all
I would like to eventually incorporate one of TI hi precision A-D's into a general A-D board, and wanted to start using the ads8361evm board - could I
just clarify the other…