Part Number: 66AK2H06 Hi experts,
My customer is running Linux on a 66AK2H06 ARM. Recently, upgraded the Linux Kernel Version from 3.10.72 to 4.19.94, but a problem is occurring with PCI. Regarding Linux updates, instead of updating only the kernel, we…
Hi Shankari G,
Sorry for late reply.
Thank you for your detailed information. We will review the information and respond to any areas that we can investigate.
O.H said: Could you tell us the conditions under which the DDR3BRESET signal is released?
Could…
Part Number: 66AK2H06 Dear Sir.
I install CCS (9.3) under Linux, and try to compile the sample code from TI. This sample project is from pdk_k2hk_4_0_16 package.
However, it shows the compile error. Not sure, how to process it. please help.
here is the…
Part Number: 66AK2H06 Other Parts Discussed in Thread: SYSBIOS ARM has a program and directly access PCIE memory and grab the data. However, reading speed is very slow.
How do I improve it? it is around 8 MB/sec.
Thank you,
Yao-Ting
Part Number: 66AK2H06 Hello,
the Network Coprocessor for Keystone Device's User Guide (SPRUGZ6) shows the reset value of the CPSW Configuration Register (CPSW_CFG_REG) as 0x00000606, linked to packet DMA channels 22 and 23. The 66AK2Hxx has 4 ethernet…
Hi Jeong,
Yes, for OMAP L138 this support is available. but, In Keystone 2 devices, it is not available in the source code.
Jeong Sang Gi said: So far, I have found a way to wake up dsp like omapl138 without using IPC .
Now I think it is correct to use…
Part Number: 66AK2H06 Hi, My customer is using 66AK2H06DAAW2 for production. Due to recent supply shortage, they are looking for pin-2-pin replacement. I knew 66AK2H06DAAW A 2 was possible device, but this is also difficult to get. I checked datasheet and found…
Part Number: 66AK2H06 Hello!
We are in process of bringing up custom board with 66AK2H06. Though we looked at EVMK2H for reference, our design does not copy evaluation board one to one.
Consider clock domains as per http://wfcache.advantech.com/www/support…
D ear Customer,
Apologies for the delayed response and thanks for your patience. Glad to hear about the consideration of K2H device for new design. Some of our multicore-support-collaterals were under maintenance and getting updated.
1. As per the "Spec…