Part Number: ADC-RTD-CONFIG-CALC Other Parts Discussed in Thread: TINA-TI Hello guys,
I am designing a signal conditioning circuit for RTD ( PT100 sensor)
I designed the circuit and got DC analysis graph Voltage vs resistance as linear
I want a graph between…
Part Number: AM6442 I saw (+) Bin Liu's Profile - Bin Liu - TI E2E support forums exchange wrt GPIO being able to be triggered on both edges as per the TRM sec 12.1.2.1.1
Now I am looking into TRM section 12.1.1 on the ADC,
BUT, I am trying to take…
Part Number: TM4C1294KCPDT Hello team.
On Figure 15-7, diagram shows tthat, Rs is needed for ADC antialiasing filter.
Looks like the value of Rs is written on the Table 27-44, which is 500Ω.
Is Analog source impedance of 500Ω = Rs of ADC input filter…
Part Number: AM263P4 Other Parts Discussed in Thread: SYSCONFIG Hi Team,
I checked the TRM but couldn't find how ADC_CAL2 or ADC_CAL3 can be used as an input channel for ADC resolvers? Also seems sysConfig still doesn't support that mode.
Regards…
Part Number: TLV320AIC3100 Hi,
What is the input Signal level (Amplitude)of CODEC IC from MIC interface ?
Can we give the input signal voltage range up to AVDD of CODEC from MIC ?
Mani Selvam P
Part Number: TMS320F28377D I am currently developing a project using the 28377D MCU.
However, I am encountering challenges in utilizing the 16-bit ADC,
particularly when dealing with single-ended analog input signals.
My hardware's analog inputs are…
Part Number: ADS7028 Hi,
I am looking at the ADS7028 for a new project. I like the part for having built-in averaging and RMS voltage capture capabilities. Would there happen to be a similar part that can accept a differential input signal? The signal can…
Part Number: AFE539A4 Hello,
I am experimenting with the AFE539A4EVM and want to get confirmation on proper configuration to achieve different ADC V_FS (full scale analog Input) as shown in table.
It appears that when set for Hi-Z Input Mode and 4x…
I tested on my f28p55x control card and found some pins' ADC data are incorrect, while some other pin's ADC data are correct.
Further investigation found the ADC data of those ADC input pins which can also be used as GPIO are incorrect, such as…