Part Number: ADC-WB-BB The containerized ADC-WB-BB is a convenient packaging of the Minicircuit balun it uses. I am wondering if you offer a similarly packaged product, but using Mini Circuits or other baluns that extend down to .2 or .4 MHz.
Thanks! …
Part Number: ADC-LD-BB
Hi Experts,
I know that ADC-LD-BB balun board is generally intended to use for single-ended-to-differential signal conversion with ADC1xDxx00RB. But is this also okay to use the other way around?
Please confirm. Thank you.
Regards…
Part Number: ADC-WB-BB Hi TI,
Does the ADC-WB-BB board have any 3D/CAD model in STEP/IGES format?
I need to design it into my chassis along with other stuff.
Part Number: ADC-LD-BB How can i calculate the value of input capacitor to ADC-LD-BB balun transformer please give clear details with calculation formula
Part Number: ADC-WB-BB I would like to know if this is compatible for my application. I have an 80 MHz 100 Ohm double ended signal that needs to go into the NI 6674T (which is single ended, 50 ohm). Will this successfully impedance match the signal? Also…
Part Number: ADC-WB-BB Hi,
I have purchased two of these converters to measure the insertion loss of twisted pair telephone wire at different length. The result I am getting does not look anything I expect. For my testing I use a network analyzer (a spectrum…
Hi,
I need to design a PCB with SMAs that match the pitch of two female SMAs (differential ends) of ADC-WB-BB as I plan to connect my PCB to ADC-WB-BB board using SMA male-male adaptors, without SMA cables.
Does anyone know the pitch between two female…
Other Parts Discussed in Thread: ADC-LD-BB Hi,
The data sheet link for the ADC-WB-BB balun says that this balun operates from 400MHz-3GHz (http://www.ti.com/lit/ug/snau123/snau123.pdf), whereas the TI page states that it operates from 4.5MHz-3GHz (http…
James:
I think the confusion related to Vcm input/output is because the datasheet is using the same term to refer to two different areas. The Vcm pin 24 is an input. This input pin accepts the common mode voltage typically supplied from the ADC. That…