Part Number: ADC08100 Other Parts Discussed in Thread: ADC3542 We are looking to evaluate the following parts to establish suitability in our next design. Could you please suggest evaluation boards we could use to conduct our analysis:
ADC08100CIMTC
ADS4…
Part Number: ADC08100
Hello. I am currently testing a design using your ADC08100 converter. The ADC data is processed by an FPGA, that takes sums 24576 consecutive windows of 3072 samples.
I am, however, experiencing an unusual noise on the data, and…
Part Number: ADC08100 Hello everyone,
I am using the ADC08100 converter for an application with an FPGA as the main processor. I want to understand the data output hold time of the ADC, which the datasheet specifies as typically 4.4ns. Do you have a…
Part Number: ADC08100 Hello,
Is it possible to create the IBIS model for the ADC08100?
I need this model to simulate the timing between an FGPA and the ADC, depending on the PCB characteristics.
Thank you in advance.
Best regards,
João Rego
Part Number: ADC08100 We want to reduce the power consumption of the ADC08100. Is the ADC08100 powered with 2.5 V a little less power consumption than the ADC08100 powered with 3 V?
Part Number: ADC08100 Hello, I am planning on interfacing with the ADC08100 with an FPGA. The sampling frequency is 100 MHz and I was analyzing if timing is stable and met.
However, after looking at the values of the datasheet, I am finding very difficult…
Part Number: ADC08100 Page 18 of the ADC08100 Datasheet states that the clocks from 20Mhz to 125Mhz will work well.
We have an option of running the device at 20MHZ (preferred) or 40MHz , is there an advantage in running the device at 40 Mhz or is there…
Part Number: ADC08100EVM
Hello, I'm planning is to use both TMS320F28374DPTPT and ADC08100CIMTCX.
It is my first time using the ADC08100. May I ask some questions.
Q) The ADC08100 datasheet says:
Although the ADC08100 is tested and its performance…
Part Number: ADC08100 Other Parts Discussed in Thread: ADC081S051 Hi ADC team
Can I get information about ADC081S051CIMF CDM(Charged Device Model) on ESD?
We knew which HDM(Human Body Model) is 3500V on ADC081S051CIMF
Best Regards
Gerald