Part Number: ADC08DJ3200EVM Hi everyone!
I'm trying to connect an ADC08DJ3200EVM to a KCU105 from Xilinx using the FMC connector. I have a FCM+ to FMC transposer allowing me to connect the two of them, in my configuration, I only use 8 lanes so the other…
Part Number: ADC08DJ3200EVM Hi everyone!
I'm trying to do a project using the JESD204 IP. I will eventually be plugging the ADC08DJ3200EVM to the IP, but at the moment I'm only working in simulation and loopback at the moment. I modified the code a little…
Part Number: ADC08DJ3200EVM Other Parts Discussed in Thread: ADC08DJ3200 Hi everyone!
We have a project where we want to connect an ADC08DJ3200 to an Artix7 FPGA. An other team has begun making the final board with the correct FPGA and the ADC but in…
Part Number: ADC08DJ3200EVM Other Parts Discussed in Thread: ADC12DJ3200EVM , ADC08DJ5200RFEVM Hi,
I just ordered the ADC08DJ3200EVM and TSW14J10EVM to connect these to a KC705. I just saw that the adapter is only included with the ADC12DJ3200EVM, and not…
Part Number: ADC08DJ3200EVM Other Parts Discussed in Thread: TSW14J57EVM , ADC12DJ3200 Dear TI, I have ADC08DJ3200EVM ADC evaluation module connected to TSW14J57EVM Data capture generator. I'm using JMODE5 Serial Data mode in single channel opera ting…
Part Number: ADC08DJ3200EVM Dear TI,
it seems that the EVM board ADC08DJ3200EVM has connected only the single-ended input to the ADC. Differential inputs INA+ and INA- are disconnected by jumpers R1/R179 and R4 at the balun1 output. In the manual it doesn…
Hi Emir,
Sorry for the delay. Yes, you need to configure the EVM to use a differential signal. Please use DC blocking capacitors and the common mode DC voltage will be fine. Otherwise, if you plan to connect a signal or pulse generator to the EVM and…
Part Number: ADC08DJ3200EVM Hi,
I bought a ADC08DJ3200EVM , and I want to use the FPGA board designed by myself to capture the data from ADC08DJ3200EVM . The input data is sine wave with 300MHz 200mV. I select Fs =1000 MHz MSPS as the onboard Fs selection…
Part Number: ADC08DJ3200EVM Other Parts Discussed in Thread: ADC08DJ3200 Hi,
my customer is planning to use the ADC08dj3200evm at lower sampling rates. Is it possible to set the sampling rate to a user-defined rate (e.g. 25 MS/s)?
Regards,
Roland