Part Number: ADC09QJ1300-Q1 Other Parts Discussed in Thread: ADC12QJ1600 , , ADC09QJ1300 hi,
The AMI simulation model for ADC09QJ1300-Q1 on TI's official website is ADC12QJ1600. Can ADC09QJ1300-Q1 also be used? If not possible, could you please help…
Part Number: ADC09QJ1300-Q1 Tool/software: Hello, we encountered some issues during the use of the ADC09QJ1300-Q1.
Mode Selection: JMODE3/8 - Stability: The JMODE3/8 mode provides stability during signal collection, including empty signal (noise) and…
Part Number: ADC09QJ1300-Q1 Tool/software: Table 6-16, 6-17 and 6-18 in the data sheet does not show the max for the input clock range for JMODE 5. The non-Q100 version of the data sheet shows this max at 1040 MHz. I'm supporting an application which…
Part Number: ADC09QJ1300-Q1 Other Parts Discussed in Thread: LMK00304 hi TI engineer:
I am having some problems with the ADC adc09QJ1300-Q1.My electrical connection is shown below
The corresponding value of the sequential address of my register…
Part Number: ADC09QJ1300-Q1
Hi Team,
Pin configuration: PD is configured for default pulldown, PLL_EN, PLLREF_SE is pulled high by default, and external clock is selected as 50M signal input. The register configuration address and register values…
Part Number: ADC09QJ1300-Q1 Hi team,
I have some questions about ADC09QJ1300-Q1 as below. thanks
1. Is the sampling rate 1.3GSPS / @9bit per channel?
2. Can I use ADC09QJ1300-Q1 If FPGA Transceiver speed is 12.7Gbps ?
3. PADC09QJ1300AAV will announce…
Part Number: ADC09QJ1300-Q1 Other Parts Discussed in Thread: LMK00304 , TPS22917 Hi expert,
I am new to ADC devices, and the customer has several questions about the device application, please kindly find below questions,
1. The output pins of ADC09xJ1300…
Part Number: ADC09QJ1300-Q1 Hi, TI's experts.
I had some difficulties with my project. I am trying to connect ADC09QJ1300-Q1 to ZYNQ-7000(xc7z100) on my board.
The circuit block diagram is same with 《adc09qj1300-q1.pdf》 Figure 9-1. Typical Configuration…
Part Number: ADC09QJ1300-Q1 Other Parts Discussed in Thread: ADC09QJ1300 Dear teams,
My customer is using ADC09QJ1300. They are not understanding following sentence in the DS 9.2.1.3: A sub-sampling technique is used to interpolate data points to form…
Part Number: ADC09QJ1300-Q1 and have a problem on debuging jesd204 interface.
Hi There,
Customer is working on jesd204 interface debugging.
Test condition: adc09qj1300-q1 which is the data transmit end. And also data receive end is FPGA, xilinx…