Part Number: ADC104S021 Other Parts Discussed in Thread: ADS1018-Q1 , ADS7954-Q1 Hi Team,
In order to more rigorously identify the appropriate ADC model, please help confirm the following problems with Customer, Thanks. 1. From the datasheet, it can be…
Part Number: ADC104S021 Page 5 describes T_CLH as the hold time between SCLK Low (which I assume means the falling edge) to CS_N Falling Edge. The timing diagram (Figure 5, Page 7) Shows t_CLH to be the delay between the falling edge of CS_N and the rising…
Part Number: ADC104S021 I am trying to save pins in my project. One option I'm considering is to try to run the ADC104S021 without active CS_N control (either by hard tieing it to ground, tieing it to a power-up reset chip, or by tieing it to a one-shot…
Hi Rain,
the specified minimum clock frequency of ADC104S021 is 800kHz and the maximum aquisition time is three periods of 800kHz which is 3.75µs. So, the LMC7101 seems to be not fast enough for this ADC.
Kai
Kris-
Thanks for getting back to me so quickly.
I am getting TXFFST != 0 in the ISR.
If I check for TXFFST==0 in the interrupt handler and just set TXFFINTCLR=1 and PIEACK.all |= 0x20 if there are still characters in the buffer without deasserting…
Part Number: ADC104S021Q-Q1 IC: ADC104S021Q-Q1 (error parameters DNL=+/-0.4,INL=-0.4...+0.3,offset error=+/-0.4. FSE=+/-0.7)
when ADC104S021Q-Q1 convert an analog singal to ADC,wo can get the typical ADC value,but how can i calculate the max /min value…