Part Number: ADC121C021
I use two ADC121C021 for sensing temperature.
When I only connected pull down resistor to VIN of the chip, I2C communication is not problem. I2C operate normal.
However, when I connect temperature sensor and read the ADC, there…
Part Number: ADC121C021 Other Parts Discussed in Thread: TPS22917 We are using the ADC12C021 similar to that shown in "ADC121C021: Oddly sensitive to value of capacitor on VIN" but with the battery voltage taken directly from the "HALF_BATT" location…
Part Number: ADC121C021 Hello,
What is the variation in the readout of ADC121C021? (Variation of the ADC alone, excluding the analog input circuit)
For example, if the analog input value does not vary by even a few uV and the expected readout value is…
Part Number: ADC121C021 An 8-channel MUX is connected to the input of the ADC121. The ADC is using auto mode and the MUX channels are switched every 1ms before reading out with SDA. I would like to ask about the disadvantages of increasing the sampling…
Part Number: ADC121C021 Hi,
I am using a circuit that combines your TMUX1308QBQBRQ1 and ADC121C021QIMKX. Is it possible to eliminate the external capacitor on the VIN side of the ADC121C021 and substitute a capacitor on the input side of the TMUX for…
Part Number: ADC121C021 We're bringing up a new design using the ADC121C021, and we're having difficulty communicating with it over I2C at 400 kHz, but 100 kHz is okay. The first thing I thought of was to check the bus waveforms, but they look…
Part Number: ADC121C021 Other Parts Discussed in Thread: TLV8541 We're using the ADC to measure the voltage of an LFP battery. We divide the battery voltage by 2 and buffer it with an opamp, followed by an optional RC lowpass. The ADC is powered from…
Part Number: ADC121C021-Q1 Hi team,
Could you advise maximum delay time from the power up to I2C communication ready?
I would like to know how long should I wait to be ready to access I2C.
regards,
Part Number: ADC121C021-Q1 Other Parts Discussed in Thread: ADC121C021 Hello,
What is "Tconvert"? The device converts periodically in automatic conversion mode. The intaerval is determined by Tconvert. But I cannot find what or how long it is in the datasheet…