Part Number: ADC121S101EVM
Dear Technical Support Team,
This website provides ADC128S102EVM-PDK-GUI for ADC121S101EVM.
PDK requires PHI board, however ADC121S101EVM requires MSP430 launch pad(F5529LP).
www.ti.com/.../ADC121S101EVM
Could you provide correct…
Part Number: ADC121S101EVM Hi Experts, Our customer would like to get more info on the pinout of the ADC121S101EVM module and the way of connecting the on-module pin headers because he said that the user guide is not describing this. He already checked the…
Part Number: ADC121S101EVM Hi TI-team
The customer wants to know how to use ADC121S101EVM.
They haven't been able to get AD values after page 11 of the user guide.
When they checked the evaluation board, the CLK was fixed to the ADC, and the CS was…
Part Number: ADC121S101EVM Hi TI-team
Can ADC121S101EVM be used on windows10 ?
(I used it on Win10 first, but the PC could not recognize the evaluation board, but I could recognize it when I changed to win7PC)
Best Regards,
Koji Hayashi
Hi Sobue-san,
we usually do not develop and offer dedicated EVMs for the Automotive (Q100-qualified) versions of our data converters. However you could order the ADC121S101EVM which can be used to evaluate the ADC101S051-Q1 as well.
Regards,
Part Number: TMDSEVM6678 Hello,
I am using TMDSEVM6678LE DSP board and have Processor SDK 5.2 installed. I have an ADC121S101EVM for sampling at 1MHz which supports SPI clock at 10-20 MHz. I need to send data from ADC to the on-board Xilinx FPGA on C6678LE…
Hi Mandar
If you want an ADC board compatible with the C2000 Piccolo LaunchPad platform then you should look at this site:
https://www.ti.com/ww/en/launchpad/boosterpacks.html
I would consider something like this one:
http://www.ti.com/tool/adc121s10…
Hi Mike,
Thanks for the feedback.
Michael Stout said: I assume you are talking about the ADC121S021 .
Yes I'm talking about this part
Michael Stout said: There are two ways you can do this.
Well, I prefer to do as you suggested at point 2 to avoid …