Part Number: ADC124S101EVM Hi,
I'm trying to set-up a new ADC124S101EVM using the user guide but I'm not able to find the link to software/GUI on the webpage for ADC124S101EVM. I've tried different browsers too. The user guide mentions that the…
Part Number: ADC124S101EVM Hello,
I am trying to use the ADC12xS10x software. A picture of the error is below. The ADC124S101EVM web page doesn't say LabVIEW is needed to run the software. Is there something else I could do to fix the errors.
Tha…
Part Number: ADC124S101EVM Hello Team,
can you share the schematic of the ADC124S101EVM with higher resolution?
The one included within the pdf is not well readable due to the data compression.
Thanks,
SunSet
Hi Tom,
Thanks for your confirmation. Probably you would like to remove "ADC124S101EVM" from ADC122S021's product folder and also remove ADC122S021 family from device support description in ADC124S101EVM's product folder description.
…
Hi Atiyeh,
There is not one code that will sweep a set of output voltages. New codes need to be written to change the output voltage.
There is a toggle mode that lets the TRIGG pin toggle between two DAC codes:
These two threads about similar GUIs suggest…
Jonathan
It seems you have indeed caught some mistakes in the bill of materials. I predict these mistakes were copy paste errors from the ADC124S101EVM, apologies for the confusion.
1. J1 is an 9x2 position header, with 100 mil spacing. I did a search…
If I go to this product page: www.ti.com/.../toolssoftware , "Software" is grayed out and I can't get to any software from there
If I go to the eval link you included ( www.ti.com/.../ADC124S101EVM ), there is no software section. When…
Hi,
I Updated my code as reading multi channel without CS changing state. But my read values are seem as shifted. For example I see Channel-4 Value at Channel-1. I am sending my code and signals at below. Please check and suggest me what I should do.
…
Hello Hai,
On the ADC124S021 EVM web page ( www.ti.com/.../adc124s101evm) download the software file and install the software. If you have used the default installation options there is some sample code in zip file that is in the Firmware directory:…