Part Number: ADC12D1800RFRB Hello, we are trying to use ADC subsystem ADC12D1800RFRB and I have a question related to the gain or scale of the output signal. I apply a 50-100mV input pulses from the generator, I also see the output pulses of correct width…
Part Number: ADC12D1800RFRB Dear all,
I am working with the reference board ADC12D1800RF (the one who has the FMC expansion connector) and I have the problem that the I and Q channels are not synchronized as viewed in the Wave Vision software, i.e., there…
Part Number: ADC12D1800RFRB HI,
I trying to capture data from ADC via ML-605. When i using Pin trigger in the TI GHz ADC the data that I captured is not capture the same time.How can I do it?. Or can I use the time stamp or not?
Thank you,
P.
Part Number: ADC12D1800RFRB Hi there,
I'm working on ADC12D1800RFRB/NOPB Reference Board. The board has 4 analog inputs: VInQ+, VInQ-, VInI+ and VInI-. On the PCB, the I-channel input connectors are labelled differently from the Reference Board User's…
Part Number: ADC12D1800RFRB Dear All,
I need to be able to digitise an RF signal at a minimum of 1 GS/s, process the samples (in an FPGA or CPU), and stream the result to a computer at a rate of at least 1 Gb/s.
Is it possible to achieve a transfer rate…
Part Number: ADC12D1800RF Hello,
WaveVision 5 does not capture the output spectrum of ADC12D1800RFRB on the external clock mode.
The software showed that the sampling rate was 0.064 MHz.
I measured the board with an external clock on May 2017, and successfully…
Part Number: ADC12D1800RFRB Good day.
I was using Wavevision 5 to acquire from ADC12D1800RFRB that I bought last year, but I had been acquiring a fs/4 signal that I do not wish. I tried to avoid this noise frequency from my application and I inserted…
Part Number: ADC12D1800RFRB Tool/software: Starterware Hello team From the Japanese university, a question came. Why can the WaveVision 5 Software not recognize ADC12D1800RFRB hardware definitely. He expects to use ADC12D1800RF in DESCLKIQ Mode. Of the following…