Part Number: ADC31JB68EVM Other Parts Discussed in Thread: TSW14J58EVM I have received the eval boards, got the them setup, and all software installed. The ADC31JB68EVM is detected by the ADC31JB68EVM Configuration GUI, but in the HSDC Pro software I…
Part Number: ADC31JB68EVM Hi Experts,
It isn't clear from the documentation if the evaluation board supports FMC connectors with low pin count. Our customer would like to use it on an FPGA development board with a low pin count. Is the FMC LPC or…
Hi Corey,
Were you able to verify that the EVM is working properly in the default mode? Do you still require assistance with this issue?
Best Regards,
Dan
Part Number: 66AK2L06 Other Parts Discussed in Thread: RFSDK , , ADC31JB68EVM , DAC38J84 Hi,
We are trying to use 66AK2L06 on TCIEVMK2L to capture ADC output through JESD204B, There is no problem running RFSDK demo by selecting 1x1-2xLTE60-HC-JESD121121x…
Part Number: ADC31JB68EVM Other Parts Discussed in Thread: ADC31JB68 , XEVMK2LX , 66AK2L06 , TSW14J57EVM , Can we connect 2 x ADC31JB68 EVM to XEVMK2LX?
Any guidelines for the connections?
Part Number: ADC31JB68 Hello,
I am testing the ADC31JB68EVM with Xilinx ZCU102 board (FMC HPC1).
But I can read only serial S0 data from the JESD204 IP core output data, S1 looks random data pattern.
Also, I found readout data look jumps. I've attached…
Part Number: ADC31JB68EVM Hi,
I am using ADC31JB68EVM and using a RF generator for the input signal. I have set the input signal to 210 MHz 0.0dBm. But on the HSDC Pro the SNR, SFDR, SINAD, THD, ENOB do not match.
what should be the other settings of…
Part Number: ADC31JB68EVM Other Parts Discussed in Thread: LMK04828 What parts need to be added/removed to configure the ADC31JB68EVM for Jitter Cleaner and Clock Multiplier Mode (PLL1 + PLL2) using a on-board XO at Y1/Y2?
Hello,
I'm starting to use the ZC706 EVB in conjuction with ADC31JB68EVM.
I've read the thread and I've the TSW14J10EVM as interpose board between the ZC706 and ADC31JB68EVM,
I need two lane and no AC so the board seems to me compatible as…