Part Number: ADS1015EVM-PDK Other Parts Discussed in Thread: ADS1015 Hello E2E,
Please let me know about the ADS1015. What is the ENOB of ADS1015?
Best regards, Puteri
Part Number: ADS1015EVM Hi,
Some questions from a beginner who started it's first steps, please assume that I would like to work only with 5V DC:
The pin numbering on J2A is not clear enough for me, where is '1' and where is '10' on the board? Where…
Part Number: ADS1115 Hi,
i need to debug to get the result for customer. so could you help me?
Where could I get the ads1115evm-pdk-plug-in-1.0.0.exe? When i download this from the ti.com, then the interface below shows.
about other information:
thanks…
Part Number: ADS1015EVM Debugging some strangeness in conversions, I decided to implement the ADS1015 ALERT/RDY line for an interrupt-driven method of reading the results register in both auto and manual conversion mode.
I have set the config register…
Hi Marvin,
Available design and development resources for the ADS1014 can be found here ADS1014 data sheet, product information and support | TI.com
The EVM for the ADS1015 might be a useful tool ADS1015EVM-PDK Evaluation board | TI.com , the schematic for…
Hi Anders,
It appears that EVM motherboard was not programmed by the contract manufacturer that built the EVM boards. So once the EVM is plugged in, click on the File menu in the GUI and select Program Device. You should see a popup showing buttons for…
Hello,
We are actually in the works to release an EVM for this family of devices, but will likely not be available until early next year.
In the mean time, the ADS1015EVM should show comparable performance.
Regards
Cynthia
Anitha,
I'm sorry, but we generally do not build behavioral models for our ADCs. For certain SAR type ADCs, we have build some models showing the sampling capacitor sample and discharge to model the type of amplifier buffers required for driving inputs…
Hi,
I wasn't entirely clear on the setup that you were describing. Let me describe the conditions that I think you're asking about and you can follow up with another question if I've misunderstood.
For the ADS1015, if the device selects…