Part Number: ADS1113 Requesting following information on Digital Filter topology used in ADS1113 ADC. 1) Type of filter used and it's order.(FIR/IIR - Sinc or other) 2) Will this filter response results in Moving average or Weighted average 3) Filter…
Part Number: ADS1113 Hi Experts,
A customer is having trouble using this part for their design.
If they set the address to 0x48/0X49, the part works well, but if they connect the address to SCL/SDA (0X4A/4B), the part doesn't work.
In the datasheet…
Part Number: ADS1113 Other Parts Discussed in Thread: ADS1114 , ADS7142 , ADS1191 Hello,
I am considering the ADS1113 ADC for an ECG application. "Continuous mode", I believe, is the best fit. However, how is it insured that the Host uP reads a 'fresh'…
Part Number: ADS1113 Hello, If I have a project working with ADS1113IDGS , I can just solder a ADS1113BQDGSRQ1 without modifications in the firmware of the project? They are 100% firmware compatible? Greetings
Hi Shuang,
You are correct. Temperature impacts gain error and how it does is shown as the gain error drift spec. So for maximum error, you will need to use the maximum gain error value of 0.15% as well as the maximum gain error drift which is 40ppm…
Part Number: ADS1113 Hello:
We have a prototype where we are using the ADC1113 to read a linear potentiometer. The potentiometer is in a very simple voltage divider configuration as shown below, measuring from AIN0 to AIN1 (or AIN0 to GND):
We have…
Part Number: ADS1113 Hello all,
We want to use ADS1113IRUGR in one of our projects. Can you please suggest if we can give 5.5V to VDD. And is the VDD voltage also same for a Vref as this IC has internal reference but datasheet wont gives fixed value of…
Part Number: ADS1113 Hi all,
Section 8.1 of the ADS1113 datasheet lists the noise performance of the device for a VDD=3.3V. How would the noise voltage change for a different VDD=5V, if any?
Thank you for your time and I hope back from you all soon…
Part Number: ADS1114 Other Parts Discussed in Thread: ADS1113 , ADS1115 , Hi,
Comparing the diagram of ads1113 with ads1114 and ads1115
It indicates a significant different input structure - ads1113 has no PGA in the input. Never the less the datasheet…
Part Number: ADS1113 Other Parts Discussed in Thread: ADS1115
Hi,
I'm little confused about how to control an ADS1113. I don't know if is a hardware or software issue, so I will start with the circuit.
I tested that the multiplexer was working…