Hi Jiang,
I took a look at the new schematic.
The FSR of ±0.512V should be okay for the range you want to measure (20-100mV). FSR = ±0.256 V would work as well.
I see potential problems with having the resistor divider network at the inputs…
Part Number: MSP430AFE221 Other Parts Discussed in Thread: ADS1115 , MSP432E401Y , MSP-EXP432E401Y Hi I would like to know if the msp430 PAM board found on ADS1115 EVM be use to program like a normal TIVA TM4C123G MCU EVM board? Saw this on SBAU362 PAGE1 …
Part Number: ADS1115 (1)ADS1115 Digital Comparator (In traditional comparator mode)
How many seconds does it take from when conversion data exceeds the limit set in the high-threshold register until the ALERT/RDY pin is asserted?(Figure1 “t_high”)…
Part Number: ADS1115 Other Parts Discussed in Thread: OPA333 I want to measure battery set cell voltages using Arduino & ADS1115 in differential measurement mode. The user may put the probes across the battery cells either in positive/negative polarities…
Part Number: ADS1115 Other Parts Discussed in Thread: OPA862 , ADS1120 , ADS112C04 This is my setup for bi-directional measurement of DC battery cell voltages battery set voltages ranging from 0.1V to 600V using ADS1115 (changing gain with help of PGA feature…
Part Number: ADS1115 Hi,
In the attached datasheet, refer to the circuit diagram. Our application involves measuring both current and voltage. Is it necessary to include capacitors CA1, CA2, and CB? In our current design, the use of CB is not considered…
Part Number: ADS1115 When using ADC to measure temperature from NTC, the "mathematics" to calculate Rt can be done:
1. using only ADC values as: Rt=Rseries/((ADC_MAX_VALUE/ADC_VALUE)-1)
2. knowing voltage of the "voltage divider": Rt=(Vr*Rseries…
Part Number: ADS1115 Hi Experts,
May I know the die marking of this PN: ADS1115IRUGR??
Since we found there are different die markings among samples
One sample is “ TI 2016 ” and “ ADS1115 ”
One sample is “ TI 2008 ” and …
Part Number: ADS1115 Hello,
We ordered on a website the pcb assembly of a pcb that have some ADS1115IDGSR parts on it.
When we have been using your product, it always had your logo and the letters BOGI
The point is that this time when we receive the…