Part Number: ADS1118 Other Parts Discussed in Thread: ADS124S08 Hello,
Currently I need to interface ADS1118 to linux based system.
I need Linux driver for ADS1118 and also It will be good to have some reference example application code for it.
Could you…
Part Number: ADS1118 Is Ccm calculated the same way as Cdiff in differential input sigma-delta ADC?
Since the input is single ended, although Ccm is connected between input to GND. I think it's still acting as a differential capacitor since the signal…
Part Number: ADS1118 Hello~
There is a Figure 50. Two-channel thermocouple measurement system.
Can I change resistor value from 500R to 50R?
does it affect to thermocouple measurement ?
Hello Mr. Benjamin,
Thank you for providing the information:
The layout for the TI Design TIPD109 is on page 16. The actual gerber files are located on the TIPD109 reference design landing page or can be downloaded from this link . - ill forward this information…
Part Number: ADS1118 Hello~
I'm testing ADS1118 with arduino mega and ADS1118-master library.
Test circuit is referenced from Fig.50. Two-Channel Thermocouple Measurement System in ADS1118 datasheet.
K-type thermocouple, FSR = ±0.256V (7.8125 uV resolution…
Part Number: ADS1118 Hi experts,
Good day! My customer is using ADS1118 in BMS. They encounter an issue in testing SPI comm. RD wrote 1 to bit0, but some times read back is 1, some times read back is 0.
According to datasheet, bit0 should always reads…
Part Number: ADS1118 Hi, i would like to connect 5 Chips of ADS1118 to DSPIC33, and i didn't find any data on the SPI capacitance ? Also, do you recommend connecting that many IC chips on same SPI bus or not recommended ? Thank you
Part Number: ADS1118 Other Parts Discussed in Thread: ADS124S08
Hi,
I'm looking for a ADS1118 Linux driver. I think that probably one of the existing linux TI-ADC drivers located at linux/drivers/iio/adc could be used to handle the communications with…
Part Number: ADS1118 Hi Team,
Can you help with the inquiry below?
A customer is using the device for measuring two thermocouples as well as acquiring the chip temperature. The microcontroller communicates with this device via SPI and there are series…
Part Number: ADS1118 Other Parts Discussed in Thread: ADS1018 , ADS1120 Dear TI experts,
My customer is looking for the IC which can measure temperature with K-type thermocouple.
I found ADS1118(16bit) and ADS1018(12bit).
my customer wants to use the function…