Part Number: ADS114S08 I am using ADS114S08 for current measurement but it causes data corruption randomly. Device configuration overview: - Internal 4MHz OSC - Data format is data with CRC - Single ended - PGA is disabled - Data Rate is 2000 I want to switch…
Part Number: ADS114S08 I am designing with ADS114S08.
To measure 1~15mV, AGC is used at 128.
At 1x, measurement works well, but at 128x, measurement does not work well.
For example, when 14.4mV is input, 14.4mV is measured at AGC 1, but at AGC 128 it…
Part Number: ADS114S08 Hi team,
I would like to consult the Absolute Maximum Ratings section of the ADS114S08IPBSR manual about the impact on the device if the input signal exceeds the marked value. Difference evaluation of signals of different amplitudes…
Part Number: ADS114S08
Hello,
What is the approximate input impedance of the PGA on ads114s08? I am trying to characterize the relationship between leakage current of diodes and the potential offset.
Thanks,
Michael
Part Number: ADS114S08 Other Parts Discussed in Thread: ADS1158 , ADS1258 Hello all.
We are developing an accelerometer reader with 12 channels.
For the data convertion, we are using ADS114S08IPBSR ADC converter.
The aquisition frequency that we need, on…
Part Number: ADS114S08 Hello.
Just to be sure. It isn't entirely clear to me, so is it correctly understood that the AINCOM pin is free to use as any other AINx pin?
Are there any special requirements for using this pin?
Best
Henrik Buhl
Part Number: ADS114S08 Hello,
I'm wondering if it's possible to hook up the ADS114S08 for supporting multiple 3-wire RTDs? I see the 3-Wire hookup example from Figure 113 of the datasheet saturating the 2 available IDACs, but is it possible to…
Part Number: ADS114S08 Other Parts Discussed in Thread: ADS1148 , , ADS124S08 Hello all,
looking for (preferred Arduino/ESP32, but can port from other) C/C++ library for ADS114S08. Is any other lib compatible (like ADS1148 etc..)?
Thank you for reply…
Hello Bob B,
Thank you for your reply.
Due to out of office, i reply late to you.
We connect 100nF ceramic capacitor between junction point at which all RTD's wire meet & analog GND.
We achieve the desired level of performance.