Part Number: ADS114S08B Other Parts Discussed in Thread: ADS124S08 I have to measure 6 RTD's with 3 wire topology, typical application reccomends to use 4 AINs per one RTD (2 for IDC and 2 for AI), which means I have to use external multiplexer or second…
Part Number: ADS114S08B Hi Team,
What is the difference between the two packages?
Or can you share with me any information about the packaging of TI's products? Thanks.
Regards, Charlie
Part Number: ADS114S08B I would like to know if the ADS114S08B (version B) includes the Reference Low voltage detection.
There are conflicting information regarding the availibility of this feature in the ADS114S08B Datasheet and in the SBAA287–May2018…
Part Number: ADS114S08B Hi!
I am implementing the ADS114S08B into a custom design and am having trouble communicating with it. I have used the recommended layout with 47 Ohm resistors in series on the SPI traces and have confirmed that the pinout is correct…
Part Number: ADS114S08B Other Parts Discussed in Thread: ADS131M08 , , ADS114S08 , ADS124S08 We are working on a project that will use 4-20mA inputs. I was planning to use ADS114S08BIPBS for this but trying to figure out what the best approach is to managing…
Part Number: ADS114S08B Hello,
We are using the ADS114S08B to measure a servo's feedback pot. Frequently, whenever the servo limit switch open, it will cause the DRDY pin to stop going low and the internal 2.5V reference will go to 0V. The noise could…
Part Number: ADS114S08B Hi, Bob and the Rest of the community,
I am using the ADS114S08B. The measurement we take is ratiometric and by using IDAC. My device can be powered by 24V AC, 24V DC, and 240V AC.
The problem arises only when the device is powered…
Part Number: ADS114S08B
Hello,
We are using the ADS114S08B ADC in our design. We are using an external reference and we are trying to setup for unipolar mode of ADC operation. We are getting converted values as if it was reporting in Bipolar mode.
…