Part Number: ADS1178 For the ADS1178, MOSI and CS lines are unavailable. How can we establish an interface without these lines? Additionally, can alternative lines be utilized to connect to the MCU since we require four SPI lines? Can you please provide…
Hello Asha,
MOSI line is a no connect; does not need connected to anything since there are no internal registers inside the ADS1178. There is also no /CS line and as a result, the ADS1178 requires a dedicated SPI port with no other devices connected to…
Hello Keith,
Thank you very much for your reply and I'm sorry to be late my response. Your reply is very helpful for us.
Thank you again and best regards, Kazuya.
Part Number: ADS1178
Dear all, I did an aprentice project in my company and have some trouble with getting data out of my ads1178. I use the SPI interface in TDM Fixed position and an Arduino MEGA2560 to bitbang the spi interface. Vref is 2.5 V and Vcc…
Part Number: ADS1178 Hi,
I designing a board using the ADS1178 and was wondering if Vcom (through an Opamp) can be used as a 2.5V positive reference at Vrefp, or would it introduce any major problems?
If some of the input channels are used in a single…
Part Number: ADS1178 Good afternoon. Now, I am considering the possibility of using your ADC in the development of our company's devices. The value of the maximum instantaneous noise level of the ADC is crucial when choosing an ADC. What parameter in…
Part Number: ADS1178 Other Parts Discussed in Thread: ADS8168 We are considering using the ADS1178 on one of our designs.
Something that is not completely clear to us is if the sample rate specified in the data sheet of 52 kSPS is for all 8 channels …
Part Number: ADS1178 The datasheet of the ADC ADS1178 mentions VREFP = 2.5V, VREFN = 0V and the FSR = full-scale range = 2VREF. For 2.5V REF will the FS input voltage range be 5V? If the signal at the input is biased at 2.5V and sweeps from 0V to 5V as…