Part Number: ADS122U04 I have the ADS122u04 communicating to a STM32 and this works fine for a while, but after a random amount of time the communication stops, with a UART time out, and I am unable to get anything further from the UART. Software reset…
Part Number: ADS122U04 Hi,. I am trying to control the ADS122U044 using micropython. Each register should be read/write fine, but when I do a conversion with Singl-Shot, it returns only 2 bytes of data when it would normally return 3 bytes of data.
The…
Part Number: ADS122U04 Other Parts Discussed in Thread: ADS1248 , We are designing a board using the ADS122u04 to replace one designed with the ADS1248 and I'm stuck on configuring the IDAC. I don't seem to be able to get excitation current flowing. The…
Part Number: ADS122U04 What is the purpose of GPIO0 and GPIO1? I can see that GPIO2 can be configured as DRDY, but I can't see any use for GPIO's 0 or 1.
Part Number: ADS122U04
Hello,
I am looking at using the ADS122U04 ADC in my measurement system and I had a few questions.
We are measuring a strain gauge sensor that outputs a 0-20mA signal.
For our application the sensor will output in the range of…
Part Number: ADS122U04 Hello,
I have a question regarding ADC gain in the ADS122U04. In our system we are taking a single ended measurement using a gain of 2 and a vref of 2.048V. I am using the equation LSB = (2 x vref / gain) / 2^24, and then multiplying…
Part Number: ADS122U04 Hello Bob,
The PT100 temperature sensing circuit (Ratio metric method) using ADS122U04 is now working absolutely fine. Now I have a query related to Pressure Transducer (0.5 to 4.5Vdc Output) sensing using ADS122U04. Presently since…
Part Number: ADS122U04 Hello Bob, Thank you for replying to my earlier query regarding ADS122U04 interfacing with RTD PT100. In the same project I also need to use ADS122U04 for measuring Engine Oil pressure (in heavy vehicles) - using MEAS make M5100 series…
Part Number: ADS122U04 Other Parts Discussed in Thread: ADS1220 , , ADS122C04 Hi Expert,
Can you help clarify the difference between ADS122U04 and ADS1220?
Is digital interface the only difference? (ADS122U04 UART, ADS1220 SPI)? If not, any other upgrade…
Hello Bob,
Thank you for your inputs.
As you suggested, I did the following:-
a) After Microcontroller powerup [and initialization of UART1 (for communication with
ADS122U04) and UART5 (for sending out values to PC for debug purpose)] , I just sent out…