Part Number: ADS1230 Other Parts Discussed in Thread: ADS1232 , ADS1120 , ADS1220 , ADS1118 Hi, Can ADS1230 be used for single ended measurements with gain of 64 and 128 ? I looked at the datasheet and on page 10, it says can be used but when I look at common…
Part Number: ADS1230 Hi team,
I got a question from customer.
" we've run into a production anomaly with a digitizer circuit in which we are utilizing the ADS1230 . Pin 1 -VDD is supposed to be connected to 3.3V and as a result of a layout error…
Part Number: ADS1230 Is it allowed to leave the AINP and AINN inputs of the ADS1230 floating? Or must they be pulled down/up using resistors?
In our application we are using multiple ADS1230 converters, and it is possible that a user leaves one of the…
Part Number: ADS1230 Hi Team,
I understand SD-ADC's date rate can be very low and the range is related to ENOB. But may I ask the sample rate min and max for the ADS1230, it only gives a typical of 10/80SPS from the datasheet? Thanks.
Part Number: ADS1230 Hi,
I met a problem during I use ADS1230 to measure the output of a strain gauge. I found even the output of the strain gauge is close to zero, the AD result periodically be very high, the duration is from several seconds to several…
Part Number: ADS1230 Hello Team,
My customer wanted to have a copy of the sample code discussed in these threads below, it seems the file is transferred or deleted.
Link: https://e2e.ti.com/support/data-converters-group/data-converters/f/data-converters…
Part Number: ADS1230 Other Parts Discussed in Thread: ADS1232 Hi, expert,
My customer met an issue about ADS1230, they set the output data rate as 80SPS, and let input 1mV DC voltage, but the output data shows not 80Hz and different among chips, all the…
Part Number: ADS1230 Other Parts Discussed in Thread: CD74HC4067 , ADS1232 , I am trying to collect analog data from 10 sensors using 16 channel TI multiplexers CD74HC4067 and ADS1232. When I collect data separately from each sensor then data is correct but…