Part Number: ADS1235 Other Parts Discussed in Thread: ADS1220 , ADS131M02 Dear team,
My customer are considering to use ADS1235 for their pressure sensor(Wheatstone Bridge)
ADS1235 is good for their application but concern point is size issue. they want…
Hi Mark Fredette,
We typically do not support Teams calls, so we will continue to support you via the e2e forum
Some comments about what you are doing, assuming as you mentioned that you are using our EVM:
Please note that there is a pull-up on the START…
Part Number: ADS1235 I have several bridges in my system. I would like to share the excitation among several of the bridges - to simplify system wiring. I also would like to use ac excitation (ref figure 82 in the data sheet). So, I will have several ADS1235…
Part Number: ADS1235 Based on this circuit design, 15 prototypes were tested on power and found that the input current of the DVDD was 24mA.
One step of testing revealed that when PIN8 (RESET) is pulled to 0V, the input current of the DVDD is also 24mA…
Part Number: ADS1235 Can AVDD and DVDD be powered separately from each other to conserve power?
I.e. can I power DVDD and communicate via SPI and the control GPIOs then power via AVDD once I'm ready to convert?
Separate from the above question, we…
Part Number: ADS1235 Hello,
I am designing a PCB using the ADS1235 on the design. In the Datasheet its states to "To minimize input leakage of the measurement channel, tie unused inputs to mid-supply voltage (AVDD +AVSS) / 2 or to AVDD." Then later in…
Part Number: ADS1235 Hello. I am designing a PCB for a Strain Gauge measurement system using 2 AD8557 as buffers for the ADS1235 controlled by an STM32. I assembled 20 pcbs, but on 10 of them I get an instability error, the measurements after some time…
Part Number: ADS1235 Other Parts Discussed in Thread: ADS1260 Hello. I am designing a load cell with ADS1235 as the ADC with a pre-amplification system using AD8557 as OPAMPS, and STM32F405RGT6 as uC for this system.
I can successfully measure and change…
Part Number: ADS1235 Hello everyone. I am designing a project using the ADS1235 as the ADC for converting load from a strain gauge connected in full wheatstone bridge (amplified and filtered by AD8557 opamp), controlled by a STM32F405 MCU. The device is…