Part Number: ADS1259-Q1 Other Parts Discussed in Thread: ADS1259 Hi,
I'm using the ADS1259-Q1 part with it's own internal voltage reference. The datasheet says that I can leave the REFP and REFN pins unconnected or tied to AVDD is this case however reading…
Part Number: ADS1259-Q1 Hi,
I'm using the ADS1259-Q1 and I would like to eliminate external voltage protection diodes in the analogue inputs to save cost and any measurement error these components may cause. The only thing stopping me is that the datasheet…
Part Number: ADS1259 Hello,
I am using Pulse mode with continuous read. Everything is working well, I just can't reconcile the need for this delay with the datasheet. I am using a state machine in an FPGA, so I have good control over the timing. I found…
Hi Ferdinand Wimmer,
Thanks for providing additional information. Please let us know what you discover as you perform additional tests
Also, I would recommend in the future to just send your code as-is. It is challenging to provide support if we are not…
Part Number: ADS1259 I'm trying to use the 3 TI ADS1259 24-Bit Analog-to-Digital Converters to simultaneous sample generated 60Hz sine waves. The ADS1259s are configured for Gate Mode 3600 SPS with 3 byte Read Continuous mode. The communication is 4MHz…
Part Number: ADS1259 For an application where the ADS1259 operates on a single +5V supply and the REFOUT (+2.5V) is tied to the AINN pin.
If a low pass RC filter is placed before the AINP pin with R=50 Ohms and C=10nF (fc = 159,155 Hz), would this basically…
Part Number: ADS1259 Other Parts Discussed in Thread: ADS127L11 , , ADS127L11EVM-PDK , ADS1248 , PGA280 , REF2025 , REF5025 , REF5020 , REF6025 Hello,
I’m working on a project where we have a very mature analog design (15+ years) and we’re trying to design…
Part Number: ADS1259 I am using A/D ADS1259.
* Operating voltage is +5 vdc and ground
*using internal reference +5.5 vdc
*using external power supply for input to IN+ and IN-
I am having problems reading in full scale from +5 to ground. It's like the…
Part Number: ADS1259 Other Parts Discussed in Thread: PGA280 Device: ADS1259BIPW
Per the spec, to exit power-down mode, you would need to hold the RESET/PWDN pin high for at least 2^16 tCLK cycles, which is around 8.88 msec when using the internal oscillator…