Part Number: ADS1263 Other Parts Discussed in Thread: ADCPRO , , ADS1262 Will the ADS126 2 EVM-PDK support ADS126 3 ?
(I have the '126 2 EVM' but need to eval the '126 3 .) I plan to desolder the '1262 and attach a socket (or the '1263).
Thanks…
Part Number: ADS1262EVM-PDK Hi Texas Instrument Im using the ADS126 chip to measure very low voltages. The precision should be within 60 nV. But every time i use the intern selfcalibration command SFOCAL, the intern offset is around 150 to 350 nV. I use…
Part Number: ADS1262EVM-PDK We are planning to develop a 6 1/2 to 7 digit universal process indicator with RTD, Thermocouple and other analogue inputs (Ohms,mVolt,Volt,mAmps).So we decided to go for 32 bit ADC. After referring to the datasheet we thought…
Part Number: ADS1262EVM-PDK Hi,
I'm trying to use the ADS1262EVM-PDK to measure the output of a photodiode sensor and circuit. I have the output of the sensor circuit attached to IN0 and the mux setup via the attached image, but I keep getting a PGARAIL_N…
Part Number: ADS1262EVM-PDK
I received a new EVM today and tried to connect to ADCPro. on my Windows 10 laptop. (I've successfully done this with this machine before) I received a message "Error loading front panel" with this in Current Plugin Errors…
Part Number: ADS1262EVM-PDK Hello ,
i just want to know how to use the Offset calibration refgisters ans the full scale registres, like what are the values that should i write it in those regiters ,
and if you can please provide me with more details or…
Part Number: ADS1262EVM-PDK hello i just need some clear explanation of :
--""Conversion Delay, in MODE0 :Provides additional delay from conversion start to the beginning of the actual conversion"
-- calibrating ADC1 and why , because its…
Part Number: ADS1262EVM-PDK I would like to know if the below configuration is correct? For ADS1262 which has +/-2.5V input. We are getting counts as 0 as output.
void ads1262Init( void )
{
delayMicrosecondsT3( 65000 );
ads1262Command( RESET );
ads1262Command…
Part Number: ADS1262EVM-PDK
Just got my EVM, checked that all jumpers and switches set to defaults, tried to duplicate the noise on page 1 of the ADS1263 datasheet.
ADC1 only, shorted input at AIN0, 20Hz FIR, PGA bypass, no chop, internal ref at 2.5V…