Part Number: ADS1263 Other Parts Discussed in Thread: INA828 , ADS1256 , , ADS1262 , ADS127L11 , ADS124S08 , ADS1258 , ADS131A04 , ADS131E06 , ADS1261 , ADS1260 I am looking for an ADC for INA828 which is taking inputs from a loadcell. I would like to be able to…
Part Number: ADS1263 Hi Friends
I am trying to use ads1263 to read two different inputs simultaneously (two single ended signal) , one input with ADC1 and another one with ADC2 . unfortunately I have problem in reading ADC2 . Both adc's are in 400sps…
Part Number: ADS1263 Hello,
May I know if the REFOUT pin be able to output 2.5V if the AVDD and AVSS are supplied with +/- 2.5 V? (DVDD is 3.3V)
Is the REFOUT stable if AVDD varies about 2.5V?
I assume that the reference circuit is powered from the AVDD…
Part Number: ADS1263 Hello all!
I could not find the noise level output when pulse conversion mode is chosen. Can someone tell me? Thank you!
Is this fixed?
Can this be changed by choosing different filters in MODE1 register, and DATA RATE in MODE 2 register…
Hi Kenny,
Without getting too deep into the details of how the ADS1263 is designed, suffice it to say that a changing input signal also changes how much current the PGA requires. As such, the current drawn by the supplies (AVDD) changes as well. In the…
Part Number: ADS1263 Other Parts Discussed in Thread: ADS1261EVM Hello Guys,
I took a task to design a system to detect 0-1.11mv voltage with resolution of 78nV.
From my side, I plan to adopt ADS1263 to handle it; but I am not sure the chip can fullfil…
Part Number: ADS1263 Other Parts Discussed in Thread: ADS1262 , TIPD188 We need a stable & low drift converter with minimum of 100000 (1 Lakh) Counts and Data rate of minimum 300 SPS
We've selected this one (ADS1263)...
But I read the following…
Part Number: ADS1263 Do you notice Ferrite beads can be useful to reduce EMI noise injection from cables connected to the AINx pins or resistors+capacitors are enough as in the datasheet example?
Thank you very much and have a good day!
Part Number: ADS1263 Other Parts Discussed in Thread: ADCPRO , Hello Guys,
Good day.
A customer is measuring with the ads1263 and read out the data with the adc pro program. The setting in his ADCpro is 7200sps. The program says the data rate is 5200Hz.
He…