Part Number: ADS1281EVM-PDK I use ADS1281EVM with single power.
So -5V is not supplied.
Jumper J7-4 AVSS is open because it will be connected to the -2.5V U13 output.
AVSS in the on-board circuitry does not appear to be connected to GND.
What are…
Part Number: ADS1281EVM-PDK Why is GPIO3 high? - I want Bipolar mode.
I have the ADS1281 EVM PDK kit.
I'm using it in Bipolar +/-2.5V mode.
I've discovered on the ADS1281 EVM that GPIO3 is high, which (post inverter U8) is disabling the Regulator…
Part Number: ADS1281EVM-PDK Hi Team,
I want to set up ADS1281EVM, when I install the ADCPro and I find my computer can't install the driver, so that I can't set up the EVM. Could you help me or provide me the TI driver configuration.
Part Number: ADS1281EVM-PDK I follow the instruction manual, but I can not connect the ADS1281EVM-PDK to the computer.
Connected power + 10V, -10V, GND and +6V.
Jumpers are set by default. Installed only the program ADC Pro v.2.0.1
When connected to a…
Part Number: ADS1281EVM-PDK My customer would like to know the length/width of ADS1281EVM as this is their purchasing procedure.
As no gerber file published, we need BU tips.
Part Number: ADS1281EVM-PDK Tool/software: Code Composer Studio Hi,
I use ADS1281EVM-PDK.
The following figure is a test.(500 SPS)
Upper is a shortcut between AINP and AINN.
Lower is connecting with sensor.
The scale of sensor reading is large than others…
Hi,
You can find information about the external supplies in the ADS1281EVM-PDK User Guide. The +/-10V supplies can be attached to J14 according to Figure 7 on page 11. Without this supply, the software driver will not load and the EVM cannot be used…
Other Parts Discussed in Thread: ADCPRO , ADS1281
I am attempting to use the evaluation board and software to talk to my board that has the 1281 installed, but not all its signals exposed.
I removed the 1281 from an EVM daughter board and with jumpers…
I am trying to use the ADS1281EVM board with the MMB0 that I have from an ADS1274EVM-PDK . I downloaded the ADS1281EVM software module but when I try to load it it just gives me a "FIRMWARE NOT FOUND" then "DSP not ready" message in …
Other Parts Discussed in Thread: ADCPRO I am trying to use the ADS1281EVM board with the MMB0 that I have from an ADS1274EVM-PDK. I downloaded the ADS1281EVM software module but when I try to load it it just gives me a "DSP not ready" message in ADCPro…