Part Number: ADS1282 Hello,
We are using ADS1282 controlled by FPGA.. ADC CLK =4.096MHZ.
Powered ADC -> applied CLK -> release PWD pin -> release Reset Pin.
DRDY pin goes high and stays high;
Try to reconfigure ADC by sending 0x41, 0x0 0xD9 …
Part Number: ADS1282 I have a design were the SPI bus of this ADC is shared with an EEPROM.
The ADS1282 doesn't have a chip select. I need to tri-state the ADS1282 DOUT (pin 4) so there is no bus contention when communicating with the EEPROM. Holding…
Part Number: ADS1282-SP Hi team,
I am doing a worst-case analysis for the acquisition channel of my board.
I should repeat them in 3 conditions:
BOL Begin Of Life
BOL+Thermal drift
EOL End of Life
My using the ADS1282-SP (5962L1423101VXC), in the datasheet…
Part Number: ADS1282 The ADS1282's datasheet states that this device can be used with unipolar (0V, 5V) or bipolar (-2.5V, 2.5) analog voltage supplies.
I would like to know if it is possible to use it with an asymmetric (w.r.t. 0V) bipolar configuration…
Part Number: ADS1282 Hello,
I am currently using the ADS1282 in my design in pulse mode. The design is composed of two external multiplexers, which provide the input voltage to the ADC for both channel 1 and channel 2. During my acquisition cycle, I perform…
Part Number: ADS1282-SP The datasheet mentions that a low-jitter clock is essential for optimum performance, but doesn’t recommend any typical values for jitter. What jitter is recommended for a DC measurement (essentially a RTD temperature measurement…
Part Number: ADS1282-SP Other Parts Discussed in Thread: ADS1282 I had some questions about the ADS1282-SP.
There was a pin called sync. I saw that there are 2 modes of operation, pulse sync mode and continuous sync mode. If we use pulse sync mode,…
Part Number: ADS1282
Hello, was testing ADS1282EVM board. But I am unable to read register map default values as given in the datasheet. I read the default values as random values at every runtime.
+VA and -VA of MMB0 is connected to +15v and -15v (max…
Hi iamcra,
I checked and there doesn't seem to be any problem with reading a bit later. I want to try a different tactic. Can you implement a ramp or triangle waveform that sweeps through full scale? I think something that we know the shape of and is…