Part Number: ADS1287 Other Parts Discussed in Thread: THP210 Hello,
We would like to connect a single ended signal to the ADC. Any recommendations regarding the connection method?
What to do with the AINM input? Should it be tied to ground?
Thanks
…
Part Number: ADS1287 p5 of the datasheet says that Vrefp-Vrefn needs to be 2.5V which I would think means that if Vrefp=2.5V then Vrefn needs to be 0V. But it also says on the next line that Vrefn can be AVSS and Vrefp could be AVDD. I want to use a single…
Part Number: ADS1287 Other Parts Discussed in Thread: ADS1278EVM-PDK , ADS1278 , ADCPRO I purchased ADS1278EVM-PDK. I would like to search for some helpful software on TI FTP site
When I try to access ftp://ftp.ti.com/pub with WinSCP it requires userid and…
Part Number: ADS1287 Hello !
Please advise.
I am trying to synchronise three ADS1287 under the following conditions, but the DRDY outputs are output at different timings.
My image is that all DRDY will output at the same timing when operating in Continuous…
Part Number: ADS1287 Other Parts Discussed in Thread: ADS1282 Hi, I have a requirement to use a 0.1ppm/year stable oscillator with 4x ADS1287-s, these oscillators usually come in a 10+MHz range, What i see if I have two possibilities: A) divide the reference…
Hi Stefan,
Single Channel, 1k SPS , 18..24Bit, continuously synchronized (SAR, or DeltaSigma with SingleShot) I would recommend looking at the ADS1219, ADS1220, ADS122U04, or ADS122C04.
Single Channel, 1M SPS, 18 bit SAR ADC with QuadSPI I would recommend…
Part Number: ADS1287 Hi, due to battery saving reasons I'd like to minimize the readout time for the four ADS1287-s we are using, right now a significant amount of the wake time is used to wait out this 24 x 1/fclk time. Can we just drop this wait time…
Part Number: ADS1287 Hi,
ADS1287 seems to release about 1 years ago but full datasheet is not available on TI.com. Do you have any reason to not release full datasheet for this device? I'm asking it because the customer is interested in ADS1287 just…
Part Number: ADS1278EVM-PDK Other Parts Discussed in Thread: ADCPRO , ADS1287 , ADS1262 , ADS1278 , INA849 , REF5025 , REF3125 , ADS1263 I hope someone can please help, I am on a deadline to collect some important data ASAP: I first want to give some background…
Hi
I dont have the data as of now. We are working on it and update the data sheet soon.
You can compare the transient performance, and the data sheet shows result with ADS1287 and it is good.
Regards
Trailokya