Other Parts Discussed in Thread: ADS1220 Hello,
I am using ADS1220 in standard electric configuration to collect measures from sensors
with fully-differential signal ranging within [0-10] mV.
I use the multiplexer configuration A0-A1 and A2-A3 for…
Hello Tony,
I designed my own ADS1298-based board for acquiring signals from some magnetic sensors. So far I've played around with the ADC and have managed to configure it, run noise measurements and get the internal test signals. However, now that…
Other Parts Discussed in Thread: ADS1274 , AM3359 Hi guys
I am using a 3-axis accelerometer which can measure +-2g with noise PSD=50ug/sqrt(Hz). I have been doing some number crunching, and based on my bandwidth of interest (100Hz) the rms noise is…
Other Parts Discussed in Thread: LMP90100 Hello,
Let me Explain my problem here.
there are 16 thermo couples, I have to read all the 16 values and I have to store it in memory.
Each 4 thermocouples are connected to one cd4052 multiplexer and it…
Having designed ECG monitors for many years I will try to describe Defibrillator Protection.
Devices that electrically connects to the human body must pass Defibrillation Discharge Compliance testing to assure it does not shunt energy. In addition;…
Hello,Mike
Thanks for your reply,
Again I want help from you. Could please suggest me a best Multiplexer for this Application.
Thanks in Advance
M.Vijay Kumar
Other Parts Discussed in Thread: DDC112 Hello,
I am using the DDC112 in a photoelectric measurement circuit but am experiencing an issue with what appears to be the DValid line. Every now and again (say 1-30) system power ups, the DValid line never…
Other Parts Discussed in Thread: LMP90080 Hello,
I am using lmp90080 for reading voltage in the range of micro volts, I have one calibration meter which will produce micro volts.
The problem here i got is when I am switching on the calibration meter…
Other Parts Discussed in Thread: LMP90080 , LMP90100 Hello,
This is vijay kumar. I want measure temperature by using RTD. and I want to use LMP90080 as a ADC converter. I want to connect 3 RTD's to one LMP90080 IC. Is it possible?
If it is possible…