Hi Matt,
Thanks for your information. Other apps engineer supports SAR ADC, you can check on TI.com or start a new thread to check the latest SAR ADC, the apps engineer will respond your query. If you have any questions about ADS131M04, please let me know…
Hi Rhea Gao,
There is FW in this reference design: https://www.ti.com/tool/TIDA-010243
Installing the .exe file yields a folder structure shown in the image below. There is some DMA code in the highlighted file.
This code is written for our MSPM0, hopefully…
Part Number: ADS131M04 Hi team,
I have a customer with the below question on using the ADS131M04 in his wireless sensor project, let me know what you guys think!
"So this ADS131M04 claimed 64Khz sampling rate, but it has -3dB attenuation at 4khz…
Part Number: ADS131M04 Dear TI
The customer used MSP430 and ADS131M04 to set continuous sampling, and after long-term operation (about 6 months), the problem of sampling data confusion occurred.
The data sampling data was normal after the chip…
Part Number: ADS131M04 Other Parts Discussed in Thread: ADS124S08 I am using TI ADC part# ADS131M04. Here is the ADC configuration used. Clock Frequency= 2.048 MHz Mode = VLP Data rate = 1Ksps OSR = 1024 Channel gain = 8 to 64 (depending on customer configuration…
Part Number: ADS131M04 Hi team,
We are using a ADS131M04IPWR for an automotive high voltage sampling application.
After power up, the voltage of the whole vehicle is 0V, while the sampling of the ADC shows 800V for around 40s, then it occurs large voltage…
Part Number: ADS131M04 Other Parts Discussed in Thread: ADS131M02 , I noticed that the digital and analog current consumption of the ADS131M04 is higher than the ADS131M02. Obviously, this is because the ADS131M04 has 4 instead of 2 channels. My question…
Part Number: ADS131M04 Hello, i would like to use a single clock to synch all of my 13 ADS131M04.
on the dev board, it use the clock SIT8924BA-22-33E-8.192000.
As the dev board i put an RC filter of 51ohm with 10pF. I think i might have some rebond or…
Part Number: ADS131M04
Hello
We are using the ADS131M04 to measure mains voltage (rms magnitude, phase and harmonic components via FFT). We want to make sure there are 256 samples per cycle (coherent sampling to minimise measurement inaccuracy). This…