Part Number: ADS131M08EVM I purchased the ADS131M08EVM and I have the same issue of connection . GUI can not connect and says not supported device or EEROM ...etc.
what could be the reason?
Part Number: ADS131M08EVM On the evaluation Board , I would like to connect a full bridge. How can this be done with the 2 , 1K ohm resistor mounted on the EVM board ??
Part Number: ADS131M08EVM Other Parts Discussed in Thread: ADS131M04 , ADS131M06 , , ADS131M08 Hi:
I was doing based on the ADS131M04, but with a new requirement I had to pick the ADS131M06.
I would like to have a reference design and as I use Altium too…
Part Number: ADS131M08EVM Other Parts Discussed in Thread: ADS131M08 To read a register, the corresponding register address must be sent with the RREG command (101a aaaa annn nnnn). However, since there are only 5 address bits (0x00 to 0x1F), reading the…
Part Number: ADS131M08EVM Other Parts Discussed in Thread: ADS131M08 Hello,
I am using the ADS131M08EVM Eval Board and I'm getting an EVMEEPROM error when I try connecting to the ADS131M08 EVM software. It says to use the EEPROM Loader but I'm unsure…
Hi Sandeep Maurya,
Dale is out this week so I will be able to offer you some support
The ADS131M08 does not have an integrated oscillator, so you need to provide an external clock signal or a crystal. This is described in the datasheet, and is shown below…
Part Number: ADS131M08EVM This is my first time messing with an ADC. I recently brought the Evaluation board to try this ADC out. I downloaded the GUI and I connected Channel 0 to a 3.3V line. So when I capture the data, I should see a voltage of around…
Part Number: ADS131M08EVM Other Parts Discussed in Thread: ADS131M08 Hi team,
If I want to test the sync pin (trying to achieve synchronous conversion), can I take two ADS131M08 EVMs, connect their SYNC pins via a jumper wire or some other connection,…
Part Number: ADS131M08EVM Other Parts Discussed in Thread: TLV2252 Hi TI,
I am trying to measure the output voltage of a medical oxygen sensor (PN: OOM102-1).
The relative information is highlighted below:
Output voltage: 9~14 mV
Recommended load: >=…
Part Number: ADS131M08EVM Other Parts Discussed in Thread: ADS131M08 We purchased 2x ads131m08evm. Is it possible to connect two modules to the same computer for data collection using the GUI?
We ultimately plan to communicate with the modules via SPI…