Part Number: ADS1672EVM-PDK I am dealing with an old project and I need to have access to the ADCPro v2 Labview sources.
HI Greg, can you send me the password of the ADCPro_v2.zip file
Regards
Other Parts Discussed in Thread: ADS1675 , ADS1672 Hi all, ADS1672EVM-PDK and ADS1675REF the EVM board size of ADS1672EVM-PDK and ADS1675REF?
Regards, Toshi
Greg,
I worked around the problems we encountered with the ADS1672EVM. The problem was never solved, but we could live with it.
(In my opinion, there is some issue with the USB communication between the EVM and the PC).
We could do the necessary measurements…
Hi Tom,
I would like to make an interface between an ADS1672EVM with a FPGA Xilinx 3AN, can you provide the source code of the ADS1672EVM-PDK I think this code is usefu to setup the registers and follow a similar code procedure for programming a processor…
Other Parts Discussed in Thread: TMS320VC5507 Hello
I am writing a thesis on studies.
I use ADS1672EVM-PDK
I need to send in Code Composer Studio a start signal to ADS and gather the probs.
I need to send a star command.
I thinkt that I should…
Since you are probably powering the device from a single supply, make sure that you are meeting the common-mode input range specs. You may have to adjust the common-mode on the THS device.
You can reference the schematic for the ADS1672EVM-PDK in the…
Other Parts Discussed in Thread: ADS1672 , ADCPRO I have the ADS1672EVM-PDK and I am trying to verify the performance of the ADS1672, specifically the noise floor.
With the inputs shorted together and biased at 2.5V from the onboard Vref through R53 and…