Hi Lei,
lei zhou1 said: 1. I found duplicated Pin42 and missed pin44 in ADS4246 package, one pin42 mapping to DA2M, another pin42 mapping to DA4M, I think it is a mistake, DA4M should be mapping to pin44, is that right? Hope your answer, thanks.
Yes, DA4M…
Part Number: ADS4246
Hello,
Please advise what is the baking conditions for the ADS4246.
When baking in reel packaging, what conditions should the customer have?
Thank you.
JH
Part Number: ADS4246 We have a requirement to read two analogue input channels from some sensors at 125MSPS or possibly even up to 200MSPS. The proposed design is to use the ADS4246 device with a Zynq FPGA target
I have suggested that early prototyping…
Part Number: ADS4246 thanks for your answers so far :-
We are going to capture 2 channels from the ADS4246EVM with the TSW1400 and save the data in binary format (since it will be 1Gbyte).
I presume that the samples in the binary file alternate, ch0…
Part Number: ADS4246 My eval boards ADS4246EVM with the TSW1400 have arrived and I am trying to get the system up and running but need some help.
The instructions are to start the software, select the 422x ADC and when prompted to upload the firmware…
Part Number: ADS4246 Another question please. We will need to run multiple tests with the eval board and it would be very helpful to automate them. Is there any kind of api that we could use to control the eval software? The minimum we need to do is to…
Part Number: ADS4246 HI Is there anyway of speeding up downloads of lots of data :-
We need to capture all 1Gbyte of data but it takes something like 15 minutes to download it from the card to the PC. Can you recommend any way of reducing that time?
…
Part Number: ADS4246 We are planning to use the TSW1400EVM card to capture the ADC outputs from an ADS4246EVM ADC evaluation board.
Do I understand correctly that the HSDC Pro v5.00 software controls both the capture card and the ADC?